Part Number: AM3356 Hi Team,
Customer is using a new design with AM335x, and prefer not to have a thermal shutdown feature included in their design. In Table 9-19 of the user manual (SPRUH73Q), it shows that there is a temperature sensor enabled by…
Part Number: AM3356 Other Parts Discussed in Thread: TMDSICE3359 , AM3359 , TLK110
Hello all,
My customer is working with the AM3356 device and has reported the problem bellow. Before going into the detailed description, I would like to highlight…
Part Number: AM3356 Other Parts Discussed in Thread: PROFIBUS , HI,
IF we are using RTOS for implementing PROFIBUS with tmdxice3359_sch_3h0013_v2_1a as reference .
Whether we can use RGMII as EMAC interface or we can only use PRU EMAC.
Whether…
Part Number: AM3356 Other Parts Discussed in Thread: AM625 Hi TI
I want to make it work as an OTG (Host or Client) depending on the external connection, if you have a schematic example for reference, please share.
Also, if I open USB0_CE and USB0_VBUS…
Part Number: AM3356 Hi, experts, I'm Katsuayama.
My udev rules does not work on usb0 otg.
Contidions
SDK version: 08_02_00_24 Kernel version: 5.10.100+ Board: custom board USB port : USB0 otg mode USB LAN device: Elecom EDC-FUA2-B(ASIX AX88772B…
Part Number: AM3356 Other Parts Discussed in Thread: TPS65910 I am currently developing the am3356.
Our model does not need an SD card, so we are working on removing it.
I have one question.
If you look in hello_world.dts
&mmc1 { status = "okay…
Part Number: AM3356 I have a problem about PROFINET IRT.
When both RT and IRT devices work on the network, the ISR of Ti and To is frequently lost for IRT device. The network topology is shown below.
Have you ever solved a problem like this?
When…
Part Number: AM3356 Other Parts Discussed in Thread: DP83TC811 Hi, Exports.
I'm Katsuyama.
We are planning to use DP83TC813R as ethernet phy.
Kernel Version is 4.19. SDK Version is 06_03_00_106.
Is there a device driver for DP83TC813R. Or, "dp83t811…
Part Number: AM3356 Other Parts Discussed in Thread: WL1837 Hi expert
When we are receiving can data with high can-bus-load (e.g. 3 or 4 frames per ms) and with high CPU load average(e.g. 1.8 or higher), we get errors of data drop, overrun or frame…
Part Number: AM3356 Hi Sir/Ma'am,
I just wanted to know, how to know or check the max dram (ddr3/ddr4..) supported by a microprocessor, here AM335X without referring the data sheet.
Is there any equations or any other formulas to calculate the same…