Part Number: AM4372 Hi Team,
My customer is running for POS machine.
Please help to suggest TI processor P/N for POS will can be used to pass Payment Card Industry Data Security Standard 4.0(PCI 4.0).
Thanks.
Part Number: AM4372 We got physically access into "xdma_event_intr0" pin D24, we check and without any modyfication on register PRCM_CM_CLKOUT1_CTRL 0x44DF41000 on that pin is 25MHz but we need check the 32kHz, so if we wrote 0x44DF41000 : 0x0 - > 0x00010000…
Part Number: AM4372 Hi,
I am using TI SDK "proc-sdk-secdev-am437x-hs-evm-01.06.00.05" to build the MLO file but It doesnt work(i.e. no serial output).
Could you provide more explanation how to verify the address "ISW_LOAD_ADDR" passed to the executable…
Part Number: AM4372 Hello
I compiled the meta-toolchain-arago-tisdk, I am using the new TI SDK 9.01.
When I installed the resulting toolchain on my Linux PC I noticed it did not have the " arm-none-linux-gnueabihf-gcc" compiler. After further analysis…
Part Number: AM4372 Other Parts Discussed in Thread: SYSBIOS Hi everyone,
I am currently using Uart0 and Uart2 to communicate with 2 different devices.
This is the configuration of the Uarts:
off_board_uart0_pins_default: uart0_pins_default { pinctrl…
Part Number: AM4372 I have a Jenkins build setup to create an USB boot image and USB boot is not working consistently from the USB device. In other words, same image written to kingston datatraveler G4 16 GB USB, this works, but board doesn't bootup if…
Part Number: AM4372
Hi Support Team,
Regarding the CTRL_DCAN_RAMINIT register, My customer has a following question.
Question: When using the DCAN1 module with AM4372, is it necessary to write "1" to the "DCAN1_RAMINIT_START" field in the "CTRL_DCAN_RAMINIT…
Part Number: AM4372 We are using ti am4372 in our design. some of the onchip memory (for example 0x4802_2000 for UART1) is giving data abort while access. Why so?
I have booted uboot 2021.
When i give =>md 0x48022000 it should show data. Instead…
Part Number: AM4372 Other Parts Discussed in Thread: SYSCONFIG Hi TI
There's a request that customer wants to get feedback of schematic review on AM4372 and Power supply.
Part Number: AM4372 I'd like to design a system based on the AM4372 SOC.
I'd like the GPMC bus to be clocked with an external oscillator that has a frequency of 43.75 MHz.
Does this device support that ?