Hi kemal:
After I recompile the project, I got a 7.5M arago-base-tisdk-image-am437x-evm.tar.xz, But this arago-base-tisdk-image-am437x-evm.tar.xz put it in SDcard, it seems that it can not boot up fully.
Please check the log file, I think that there…
Schuyler Patton said: Which TI Linux SDK are you using?
Ti sdk am437x-04-02
Schuyler Patton said: Are you asking this question from a Linux or U-boot perspective?
I am not getting what you mean by that, anyway i want to check in root login prompt…
Part Number: PROCESSOR-SDK-AM437X Other Parts Discussed in Thread: WL1835 Tool/software: Linux Hi all,
I am working on am437x ti sdk ti-processor-sdk-linux-am437x-evm-05.01.00.11.
I have a custom board based on ti am437x gp evm. I am trying to integrate…
I observed build with am43xx_evm_defconfig and am43xx_pic61_defconfig for both targets.
Using make u-boot command only create u-boot image not primary bootloader image (MLO)
can you cross check ? tried different below command so for evm it created…
Hi Pavel
Thanks for your answer. I should describe more clearly.
- My system : Ubuntu 16.04 LTS; ti-processor-sdk-linux-am437x-evm-05.00.00.15-Linux-x86-Install.bin; AM437x GP EVM Rev 1.5B
- Purpose : I have a sdcard that created by create-sdcard…
Hi Manisha,
here it is.
Jiri
Fullscreen
3348.dmesg.txt
Download
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4…
This is on a custom board, WiFi is connected to the mmc2 interface. The attached file contains the boot log.
Fullscreen
5531.bootlog.txt
Download
�<debug_uart>
*********Scaling vcores****************
Getting ready to scale...
almost…
Part Number: AM4378
I have a custom AM4378 board based on the AM437X-SK EVM. There is a Micron eMMC device (MTFC4GACA) connected to the mmc0 interface.
The eMMC is not detected by Linux.
I was able to partition the eMMC using the following commands…
Fullscreen
pic6Ethernet.txt
Download
root@picv6-1:~# dmesg
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 6.1.33-g40c32565ca (oe-user@oe-host) (arm-poky-linux-gnueabi-gcc (GCC) 11.5.0, GNU ld (GNU Binutils) 2.38.20220708…
dmesg log file is attached.
we are using Cypress CYUSB201x USB controller, as a high speed USB device.
And this device detected on other board and host pc but can not be detected with this board
Fullscreen
ti_dmesg.txt
Download
[ 0…