Hi Danilo, I'm attaching a working boot log with SDK 7.3 on AM437x GP EVM for your reference. 1. From your log file, are the kernel & DTB files are ported and built based on SDK 7.3? Filename 'zImage'. Load address: 0x82000000 Filename 'CoreACE_A_B.dtb…
Hi Biser,
Thank you very much for your fast reply
Still I am unable to send or receive data
processors.wiki.ti.com/.../5x_CPSW checklist results:
=============================================
u-boot : u-boot-2016.05+gitAUTOINC+4db46a6bbd-g4db46a6bbd…
Hi Hong,
steps I did to recreate an issue:
uname -a
Linux am437x-hs-evm 4.19.94-gbe5389fd85 #1 PREEMPT Mon Apr 20 02:19:56 UTC 2020 armv7l GNU/Linux
enable no console suspend:
echo N > /sys/module/printk/parameters/console_suspend
root@am437x…
Part Number: AM4378 Hi,
I'm trying to connect LCD which has touch and USB I/F to am437x-gp-evm thru HDMI.
I attached log file. USB I/F looks like OK between LCD and evm board in host mode.
Is there any way to use USB base touch panel ?
8130…
Part Number: AM4378 Hi,
I have an AM4378 Custom. I have an error message during the boot.
[FAILED] Failed to start Load Kernel Modules. See 'systemctl status systemd-modules-load.service' for details.
Pls let me know how to fix this problem.
I…
Hi and thank you for taking time to help me.
I have this board: http://www.ti.com/tool/TMDSIDK437X
Below are the requested log files attached. I noticed one funny thing when reading through them, in the boot log i noticed that the board is loading…
Part Number: AM4378 CPU:AM4378
SDK:07.03.00.005
Kernel:5.4.106
sgx:ti-sgx-ddk-km-1.17.4948957
kernel log:
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 5.4.106+ (root@monitor1804) (gcc version 9.2.1 20191025 (GNU…
Part Number: AM4378
Hello TI Support Team,
We are facing the Hang issue on AM437x-HS board on Serial port Furius byte Rx buffer fill. Please referee the Thread created earlier.
https://e2e.ti.com/support/processors-group/processors/f/processors…
Schuyler,
Attached is a full terminal capture from power-on to prompt of the SK with the 06.00.00.07 Processor SDK. We have verified via dmesg that no additional messages are printed during the iperf testing.
Fullscreen
am437x_sk_06.00…