Part Number: CC1310EMK Other Parts Discussed in Thread: CC1310 , CC1010 Background:
I have previously built CC1310 solutions and I am looking at interfacing with a CC1010 based solution over the air. I do not have any experience with the CC1010 platform…
Other Parts Discussed in Thread: CC1010 hello to all my colleagues, I ask to help me with questions on RSSI I'm using CC1010 with HOPPING, everything works fine except RSSI, and I can not understand that there do not correctly ,
code written by me is…
Other Parts Discussed in Thread: CC1010 Hi, i am working with the old ic CC1010. I am trying to develop a UART transmitter by the air, in transparent mode.
I find in the examples, a project named "RF232", which uses the Simple Packet Protocol (SPP)…
Other Parts Discussed in Thread: CC1010 Hi,
I'm new with the CC1010 RF microcontroller... I have two CC1010, the first is configured as a transmitter and the second as a receiver. I want to transmit a byte with the first microcontroller to the second…
Other Parts Discussed in Thread: CC1010 There is a bug in the HAL if a CC1010 and is used with a 3.6864 MHZ XTAL.
Particular the functions halCopy2Flash and halFlashWritePage are affected as they calculate a to fast FLTIM to write into the flash. …
Other Parts Discussed in Thread: CC1010 Hi, I am moving a project from CC1010 to CC1110, and therefore also changing compilers and libraries from Keil to IAR. I now have the radio protocol sorted out for simple broadcasts - i.e. a CC1010 device tx is…
Other Parts Discussed in Thread: CC1010 HI everybody
I am working with the cc1010. My problem is that I have evaluation board and two evaluation modules. In swru055 I have read that PC running Keil compiler and Chipcon IDE and we can use parallel port…
Hi,
The name of the function should not matter. Are you able to configure the CC1010 ADC with this function?
What would you like the get accomplished?
LPRF Rocks the World
I see that this is an old posting but maybe someone is monitoring it and can help with my issue with CC111x compatibility with CC1010.
I have an old design with CC1010 and need to communicate two-way with a CC1111 for the USB function. To this point…
Other Parts Discussed in Thread: CC1010 Hi everyone, I am having some problems getting the analog to digital converter on the CC1010 to work through AD2.
I
have a temperature sensor which puts out a constant voltage
proportional to the temperature.…