Please see the attached text file that has many failure patterns. The first pattern of the file is
{'errors': ['0x15'], 'idx': 1, 'locations': [24], 'rx': [['0x82', '0xae', '0x8c', '0x3e', '0xf4', '0x6', '0x45', '0x87', '0x6d', '0x70', '0xdb']], 'tx…
Hi Matt,
I've done another discharge of the pack with a FCC learn up/down set at 15000mAh and the FCC updated at 63000mAh which means that he just added 15000 to the old value (48000mAh).
I think that's a normal behavior because we have a capacity…
Hi DK, Thank you for quick reply. I send the results obtained by PCIe's protocol analyzer in the unlinked situation. Could you confirm it?
We think that the timing of AM5726 link is not overlooked. Is it possible to adjust the timing? It links once…
Hello Sir,
I completed two learning cycle process. The files are attached here(Learning cycle file and export gg file)
The full charge capacity value before the start of the first learning cycle process is 12601 mah (rest-exit-rest-charge-relaxation…
Part Number: BQ40Z50 Other Parts Discussed in Thread: BQSTUDIO Hi all, We are facing similar issues when logging the register values. We did a comparison test: Connect the battery with EV2300 and use bqStudio to log the registers with only changing FLASH_BUSY_WAIT…
Part Number: BQ40Z60 Other Parts Discussed in Thread: BQ27510-G3 Tool/software: Code Composer Studio Hi TI:
My current BQ is BQ40Z60. NTC is 10k(Thinking DHT0A103F34D2SY, R tolerance=1%, B tolerance=2%).FW for temperature is like below table. Schematic…
Hi, Kang,
Yes, we have PF enabled. (VIMR/VIMA)
I am attaching two data log for your reference. (discharge test by 2Amp)
Status of Serial 5041 & 5052:
(1) Max Delta Cell Voltage: 890mV / 729mV (the initial value before storage test 276mV)
…
Part Number: BQ40Z50
Dear Sir,
When Charing, it happened OC alert. it seems RemainingCapacity() < FullChargeCapacity() is correct.
what is Internal Charge counter? if OC:Threshold is change. it is OK? There is side impact?
could you let me…
Hi OD,
For the Above mentioned screenshot's log is attaching with this reply (change file name from .xml to .subx). In the attached log IEEE addr of ti devices 4th byte is "0x0A"(ie 3C C1 F6 0A xx xx xx xx) and all other are 3rd P devices. Sniffer packet…
Supplement debug logs
[TS (START): 13.07]
===== Dumping environment info ======================================
[TS: 13.07]
Date: Thu Jan 1 00:00:18 UTC 1970
/proc/version: Linux version 5.10.162-g76b3e88d56 (ci@CI-HZV-AUTOELEC-SLAVE…