Part Number: CD74HC4051-Q1 Hi Team,
Just woudl like get the design confirm for 3.3VCC and 1.8V Channel IO(A0 to A7) is working normally? and COM OUT/IN(A) will have 3.3V as VCC level? or same as Channel IO voltage level?
BR.
Lenny Lee.
Part Number: CD74HC4051-Q1 Other Parts Discussed in Thread: TMUX1308-Q1 Tool/software: Hi expert,
Could you share the PSPICE model for CD74HC4051-Q1?
Thanks!
Ethan Wen
Part Number: CD74HC4051-Q1 Tool/software: Hi,
I need the conditions that are considered for measuring the Rthja mentioned in the datasheet.
Below are the details I am looking for:
Board type used (is it FR4)
Copper thickness of board in oz …
Part Number: CD74HC4051-Q1 Hi expert,
Since there is -24 voltage in the system, in order to avoid over-voltage damage to Ax to Gnd, can the maximum current be limited to avoid negative voltage damage to the Device? What should be the maximum limiting…
Part Number: CD74HC4051-Q1 Hi team,
I have an application question which need your help.
After the chip is powered on, what is the state of S0 S1 and S2? Does X mean high impedance? And if not, what would it be?
If the GPIO pin of C2000, which connected…
Part Number: CD74HC4051-Q1 Hi team,
How to understand the "Operation Control Voltage" and "Switch Voltage" in datasheet?
As far as I understand, "Switch Voltage = 0 V to 10 V" means the max analog signal swing through Channel I/O pin and COM pin is…
Part Number: CD74HC4051-Q1 Hi,
A customer is evaluating the CD74HC4051-Q1 and has a couple of questions below:
- What would be the propagation delay at Vcc=3.3V and Vee=GND?
- How is the jitter performance?
- There are also concerns over typical…
Part Number: CD74HC4051-Q1 Hello Team,
Can CD74HC4051-Q1 replace 74HC4851PW-Q100? The nexperia part pin 7 is NC where the VEE pin of the TI part is dedicated.
What is the function of VEE pin?
Thanks in advance.
Joern
Part Number: CD74HC4051-Q1 E2E,
What’s the max input voltage of CHANNEL I/O AX?
If the input voltage of channel 1 is higher than absolute maximum ratings, does it affect other channel?
If any diagram could help customer analyze this failure…
Hi Jeffrey,
CD74HC4051-Q1 can only support +/-5V. CD4051B-Q1 can support up to +/-10V.
Are you working on an automotive product? If not, I would recommend MUX508