Hi Huy,
I review the schematic for TPS51117 and TPS51100. Both schematics look good and only need minor changes. Here are my comments.
TPS51117: ( 1.5V and 1.8V)
1. Add 1uF ceramic capacitor close Pin10 V5DRV. This capacitor should be same as…
Dear Sir,
Vin=12V,Vreg3=3.3V,V5A=0V,V3P3A=0V,when the 51285 shutdown.There are 2 options in the schematic and we use option 1(auto power-on).
2021.UP.pdf
Part Number: BQ25731 Other Parts Discussed in Thread: BQ25730 Dear Madam/Sir,
I would like to have your eye on the design review (on PDF page 11) (P9DF page 8 is power tree)
One more question, could I direct output Vsys to PMSM Motor (24V)? rectangle…
Hi Chuck
Ok Understood...I wish there was a note in the ref design which says that "do not copy this circuit onto custom design". that way I would have been careful. Anyways....now that I know, I bought an EEPROM burner and removed the flash from my…
Hi,
The TPS25750 can be programmed using the web GUI available on TI.com. The web GUI is simplified to make the device easy to program.
Simply open the GUI and connect the TPS25750EVM to your computer via a micro-USB cable. The GUI should auto detect…
Other Parts Discussed in Thread: TUSB8041 , TPS65982 Dear Sir:
My customer followed TIDA-00630 Type-C reference design to draw circuit and PCB layout.
The different is my customer added one set of TUSB8041 (position is U37) in 2nd layer in this…