Part Number: DAC5311 Other Parts Discussed in Thread: DAC7311 Hello
I am using DAC5311/DAC7311 in our design , when I connect it to load the output is 0, without load the output is ok.
What can be the problem?
Hello TI,
We have below TI DAC driver from the kernel path "drivers/iio/dac/",
ti-dac082s085.c ti-dac5571.c ti-dac7311.c ti-dac7612.c
Which driver will you recommend us to take as reference to customize for DAC60508,
Thank you,
Prathi…
Other Parts Discussed in Thread: DRV2700 , TINA-TI , DRV2700EVM , DAC53701 , DAC7311 Hi Experts,
We've been looking for available DAC device with TINA-TI model to simulate with DRV2700.
Customer is actually looking for an input (DAC) component to…
Part Number: DAC8560 Other Parts Discussed in Thread: DAC8311 , DAC7311 , DAC8411 , DAC80501 Dear experts,
My customer is looking for smaller package device than DAC8560. They need to meet the demand below:
1、 Package;the smaller the better 2、 Power…
Hi Paul-san,
Our customer look for low power DAC in normal operation mode.
A reference device has following current consumption characteristics, Fsck is one of key parameter.
So, <10uA current consumption can be achievable at Fsck 100KHz condition…
Part Number: DAC7311EVM Other Parts Discussed in Thread: DAC7311 Hi All,
I am using the DAC7311 Evaluation Board, SPI communnication is working and it is stable.
Everything works well except that the output is always the half value of what exptected…
Dear Eugenio, thanks a lot for kind reply.
I will check with DAC7311 for my application.
I have also found a very simple solution (+possibility to do bipolar pulses) with OP Amp + digital potentiometer, like on attached photo below:
Are you just trying to generate 11steps? 0 V, 1 mV, 2 mV... 9mV & 10mV? The DAC9881 it cannot do this on its own because of its large zero code error. It will require a negative supply and an external circuit to achieve this.
I would suggest taking…