Part Number: DLPC3439 Hi TI,
I have two questions about the LABB dimming function.
I guess the dimming function is realized by adjusting angle of DMD millers through DMD Sub-LVDS signals.
Is my guess correct?
Regarding this feature logic, is…
Part Number: DLPC3439 Other Parts Discussed in Thread: DLPDLCR4710EVM-G2 , Dear all,
We developed a DLP projector based on the TI DLPDLCR4710EVM-G2 and now we are trying to make it run (hopefully perfectly).
I managed to program the on-board MSP430…
Part Number: DLPC3439 We got an external CPU connected with DLPC3439 by I2C bus, and need to on-line update the image in the SPI FLASH chip that attached on DLPC3439 with external CPU program.
The CPU program sent order to DLPC3439 by I2C bus, and then…
Part Number: DLPC3439 i want know crystal route length from 24M crystal to one DLPC 3439 and from crystal to another DLPC3439 ?
Impedance for crystal is 100 OHM, this is necessary?
I search DLPC3439 SPEC, how long the length for crystal to DLPC3439…
Part Number: DLPC3439 HI TI team:
We found DMD damage during aging of 1080p DLP projection project. The damage status is shown in the following figure.Many vertical lines
Now we need to find out the damage reason ,Please give some suggestions
Part Number: DLPC3439 Other Parts Discussed in Thread: DLPA3005 , , DLP4710 Hi,
I'm actually testing new TI firmware FWSel_DLPC3439_DLPA3005_pm2_i2c0x36_v7p7p0.img. Working just well, but compared to firmware dpp3439-dual-ASIC_7.3.2.img communication…
Hello Vivek,
I have just one issue with output range of luminance levels, otherwise complete system works perfect. Parallel interface in mode 16-bit YCrCb 4:2:2 expect full range of levels from 0 to 0xff (256 luminance levels), but my video decoder…
Part Number: DLPC3439 The moisture resistance level (MSL) of the DLPC3439CZEZ is level 3,
According to the J-STD-033D standard, it must be consumed within 168 hours after opening the package.
It is impossible for us to consume all 2500pcs of a plate…
Hello Ed,
Thank you for your interest in our DLP Technology.
The firmware is getting normally provided from our optical engine manufactures. Do you have an optical engine manufacture you are currently working with ?
Thanks,
Nadine
Hi Anyiam,
Yes. I have checked the pin-mapping between TFP401 and DLPC3439.
But I couldn't find out any problem.
On my own board, I'm using two of DLPC3439.
The master and slave of DLPC3439 are sharing the same signals from TFP401.
The signals…