Other Parts Discussed in Thread: DM388 We have a new camera sensor.
It's output is YUV422_16bit_ 720P@60(CCIR601 16bit-mode).
Our EVM is IPNCDM388(Main-Chipset "DM388").And the software is base on RDK3.8.0.0.
My question is.....
Base on our camera…
Other Parts Discussed in Thread: DMVA3 , DM385 , DM388 Our main task is video transcoding and transrating. We need to process as more channels as posssible by one device.
Currently we are using DM8168. It can transcode 16 x 720x576@25fps or 3 x 1920x1080…
Other Parts Discussed in Thread: DM388 , DM385 Hi All,
I am working on DaVinci DM388 processor , ipnc_rdk 3.80.00 and configuring it as I2C slave device.
How linux informs that it is now being accessed.as I2C salve ?
Should it have to generate…
Other Parts Discussed in Thread: DM8107 , DM385 , DM388 Hi,
I have two board, one is based on DM8107 and one is DM388, Now If i set DM8107 board to force EMAC mode it display 'DM385 ROM V1.0' in BOOTP request, I want to know the same name for DM388…
Other Parts Discussed in Thread: DM388 , DM383 , DM385 Hi!
I'm testing tmdsipcam388imx136
I try to repeat measurements according to IPNC_RDK_InstallGuide.pdf. Firware is ubifs_ipnc_low_power (also try full future ) from IPNC_RDK_V3.8.0 (dir: Binaries…
Other Parts Discussed in Thread: DM388 Hi all,
This is in concern with an issue we're facing while implementing IP Camera device using DM388 SoC and IMX136 image sensor from Appro.
We are using Sony's IMX136 image sensor with Aprro as vendor.…
Hi Ivan
1. Yes. It is booting from Linux and all the demos are working fine.
2. There is no direct TI FAE in Singapore. We are working with a 3 rd party, they don't have DM388.
It would be nice if you could provide a solution.
Thanks
JK
Other Parts Discussed in Thread: DM388 , DM385 , TPS65910 , TVP5158 Hi
I am using DM388 IPNC RDK ver 3.8(H/W rev2).
My bootargs are:
setenv bootcmd 'ipnc_ff_init 1;tftp 0x81000000 uImage; bootm' setenv bootargs 'console=ttyO0,115200n8 root=/dev…