Part Number: DP83TG720EVM-MC Tool/software: If I have the current implementation setup (867 PHY/ 720 PHY) like the media converters are back to back connected, will the gPTP synchronization signal (IEEE 802.1 AS) just pass thru the Ethernet PHYs uninterrupted…
Part Number: DP83TG720EVM-MC Tool/software: 1.) I have my design setup exactly like the DP83TG720 Media Converter module. The question is what is the physical layer end to end delays on the converter as far as data sent from one end of the PHY (720) to…
Part Number: DP83TG720EVM-MC Tool/software: Hi Team,
The customer will use DP83TG720EVM-MC to evaluate DP83TG720RWRHATQ1 system that they designed.
The evaluation is communications check by ping.
Is the attached configuration OK?
Please let me…
Part Number: DP83TG720EVM-MC Tool/software: hello team
may I have the Register configuration table, which MSP430 sends to DP83TG720 and DP83867 ? thank you!
Part Number: DP83TG720EVM-MC Other Parts Discussed in Thread: TIGER Tool/software: Hi,
Could BU provide the DP83TG720R design file in dsn formation for my customer inquiry?
Thanks and Best regards,
Tiger
Part Number: DP83TG720EVM-MC Tool/software: We found that on UBUNTU, the network is always connected when the SPE cable is removed.
However, when the SPE cable is connected, obtaining an IP address from the DHCP server takes about 3–5 minutes before…
Part Number: DP83TG720EVM-MC Other Parts Discussed in Thread: DP83TG720S-Q1 Tool/software: hi Ti Team
"I am currently using the evaluation board 'DP83TG720EVM-MC'."
"I followed the connection below and sent the register commands, but I still couldn…
Part Number: DP83TG720EVM-MC Tool/software: Hi ,
when I use USB 2 MDIO sofware configure DP83TG720 enter to TESTMODE, the sofware return value is 0000 , can you help me to solve this question? thank you very much
Hi Jim,
JIM SHEN said: Does this mean that two PHY devices must be physically connected via SPE (TRD_P/N) and in a Link-Up state before Test Mode 1 will output the 125 MHz clock?
Yes.
JIM SHEN said: Based on the datasheet, we believe that Pin 16…