Hi Bin:
I configured USB according to what is explained in the videos.
I dont see any usb error messages during linux startup.
After "modprobe g_ether", directory "/sys/class/udc" is empty,
and "lsmod" shows "g_ether" and other usb related modules…
Hi ,
There is a error about that " omap_crtc_flush() timeout " will always come out when I type modetest.
And it begin at omapdrm module initial stage......
[ 5.198501] omapdrm omapdrm.0: lcd3: timeout waiting for enable [ 5.398506] omapdrm omapdrm…
2025 FAQs
#
FAQ Title
E2E link
Domain
SoC
1
How to Set PCIe0 Transmitter De-emphasis?
https://e2e.ti.com/f/791/t/1427955
PCIe
TDA4VL/AL
2
How to boot from EMMC without SD Card and boot from SD card as well …
Hi Steve,
I have migrated my board changes to latest SDK you suggested, where we believed tuning algorithm is better.
Below is the block diagram, components used supports SDR104 @ 204MHz
As per my board & application requirement, SD/MMC controller…
Part Number: PROCESSOR-SDK-AM57X Other Parts Discussed in Thread: SYSBIOS
We have a design based on AM5701 that is currently working with SDK 06.03.02.08, we are migrating everything to SDK 08.01.00.09. However, we are facing difficulties in porting…
Hi,
Fullscreen
0284.kernellog.txt
Download
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.79-rt47-g28d73230da (ksm@ksm-HP-ProBook-450-G5) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #1 SMP PREEMPT…
Part Number: TDA2EG-17 Other Parts Discussed in Thread: TDA2 , PCF8575 Tool/software: Linux Hi,
Now I have a problem that my custom board cannot detect USB flash disk in host mode when excuted "usb start" in Uboot mode.The log is attached.
And I open…
Hi Vishal
There are my .config file and procedure message when I run sd card.
Is MPU max freqency 800?
Because I see tda2ex file table is show 800,but mpu default freqency is 1000.
thanks
Yumei
Fullscreen
6013.kernel_boot.txt…
Part Number: TDA2EG-17 Hello all,
We have custom board and are using 1G DDR based on PROCESSOR_SDK_VISION 03_07_00_00, to boot from sd or emmc.
Need early boot + late attach with our usecase(one lvds output to TFT panel) to work in 5 sec system…