Part Number: DS100DF410 Hi,
My customer is using DS100DF410 in one of our platform. They want to configure the device in 1G mode.
We have configured the device as per Ref_mode 3 Mode (Reference Clock Required).
Default setting of Ref_mode 3 Mode…
Part Number: DS100DF410 Does the DS100DF410 Retimer pass the preamble of the Ethernet packet + gap time of 12-bytes ? we are seeing 20 additional bytes for each Ethernet packet sent thru the Retimer at 10G Ethernet rate; using IXIA to generate packets…
Part Number: DS100DF410 Can the DS100DF410 be used for Ethernet 40G QSFP applications ? we have not been successful with linking to 40G QSFP ? any idea's ? the circuit uses two DS100DF410's; one for TX and one for RX.
Part Number: DS100DF410 Other Parts Discussed in Thread: DS125DF410 , DS110DF410 Hello,
I guess we could use this for QSGMII as well, or maybe you could recommend some other part.
In this design we have 12xQSGMII lines and 4x10.3125G
Could you…
Hi Honma-san,
The choice of floating A0, A1, or A2 depends on the EEPROM size and whether the voltage on these pins is used for addressing the EEPROM. Both the DS100DF410 datasheet Figure 5 and SNLA245 Table 5, 6 are valid.
Please look in more detail…
Other Parts Discussed in Thread: DS110DF111 , DS100DF410 We are using internal PRBS generator for testing. But oscilloscope show could not recovery clock.
We had configed with the sequen below:
p i2c_write_byte(0, 0x70, 1, 1) //I2C switch p i2c_write_byte…
Hi Eduard,
Is 1.7 Gbps the actual measured bitrate on the interface or the effective data throughput of the interface?
The DS100DF410 retimers will not impact the overall throughput.
The data collected in the registers indicates that the retimers…
Part Number: DS100DF410 Dear Sir, We are using the DS100DF410 component in a system that has 1.25G/10.3125G multirate ports. We are having issues with environment temperature changes when the component is at the 10.3125G data rate. The product must meet…
Hi Tom,
The DS100DF410 can be used for SR and LR applications, which do not necessarily have an EDC requirement since they are limiting modules.
However, if EDC is required to meet BER requirements and the module is a linear module (for example, with…
Hi,
we have the transmitter from the firefly optical receiver 15mm-s from the DS100DF410 input. The link speed is 10.3125Gbps. Should we change any register on the retimer at all, or it should just work with the default? :)
We don't have CRC-s on…