Part Number: DS125BR800 Hi Team,
There are two questions about DS125BR800, could you please help explain? Thanks!
1. The datasheet says "Transmit Output Voltage Control: 700 mV to 1300 mV", is the voltage peak to peak voltage or average voltage?…
Part Number: DS125BR800 Other Parts Discussed in Thread: DS125BR820 , DS125BR401A HI team,
Do we have some recommend redriver devices for SAS3.0? Thanks.
Part Number: DS125BR800 Hi all
I would like to confirm what minimum Vpp for input RX signal? According to the specification, 100mVpp is defined as IDLE threshold then I guess this IC can recieve below 100mVpp signal.
Let me know actual minimum input signal…
Part Number: DS125BR800 Other Parts Discussed in Thread: DS125BR820 , hi team,
my customer has designed a board with DS125BR820 or DS125BR800, currently we have tested the 820, and we want to get the configuration for 800. Could you please help provide it? EQ…
Part Number: DS125BR800 While creating a PCIe x8 reDriver Card, i want to use two DS125BR800 chips: one for TX and second one for RX channels. Both chips should read Equalization Info from on-board EEPROM. According Application Report SNLA228 (Page 4),…
Part Number: DS125BR800 Other Parts Discussed in Thread: DS125BR820 , Hi, We are using this part as a probe on a PCIe Gen3 link. Do you have a more detailed listing of the 256 different equalization settings? We would like to explore whatever total gain…
Other Parts Discussed in Thread: DS125BR800A , DS125BR800 Hi,
I believe that the difference between DS125BR800A and DS125BR800 is in terms of supported SAS-3 application or not. Is my understanding correct?
Best Regards,
Kato
Other Parts Discussed in Thread: DS125BR800 Hi,
We are using using DS125BR800 for PCIe redriver purpose. Is that possible to put the redriver in x1 mode only ? Currently x8 pass through is working. But if we connect x1 card it is not working. So like…
Other Parts Discussed in Thread: DS125BR800 Hi Team
Diff + and - coneect to TI DS125BR800 input iC - and +?
is it OK for design. (SAS signal - connect to + redriver, SAS signal+ connecte to redriver -)
In 2.5V mode the VDD pins are tied together to an external 2.5V rail, however in 3.3V mode, the VDD pins are supplied by the internal regulator. The datasheet recommends each VDD pin gets it's own 0.1u cap, but should the VDD pins also be connected to…