Part Number: DS280DF810 Hi team,
My customer is using DS280DF810, and they now have a requirement that after switching from straight-thru mode to cross-over mode, the relock time should be less than 4ms. Considering RXA & RXB are all 25Gbps rate signal…
Part Number: DS280DF810
Hello,
I have an application that would requires more than 9dB of boost, but less than 13dB of boost from the CTLE. Table 42 in the programming guide gives some insight into the boost ranges in the auto adaptation algorithm…
Hi Edward,
Please let me know if you have access to the DS280DF810 Programming Guide. In this document, you can find procedure for setting the device in RAW mode.
Here is a summary: There are two registers - Reg 0x1E[7:5] and Reg 0xA5 that define…
Part Number: DS280DF810 Hello,
Does DS280DF810 have link training function ? Customer request link training and re-timer integrated solution. Thank you.
BR
Patrick
Hi. The USB2ANY circuitry implemented on the DS280DF810 EVM and the DPS DONGLE respectively are essentially the same. You may if desired use external DPS DONGLE to communicate to the DS280DF810 EVM over I2C instead of the onboard USB2ANY circuitry on…
Part Number: DS280DF810 Hi,
Below attached schematic is from one of our most important customer, so could you check whether there's any potential problem or not?
M3000_RETIMER.pdf
thanks,
TS
Other Parts Discussed in Thread: DS280DF810 , DS280DF810EVM rt Number: DS280DF810
HI Sir
1. When I use PRBS15 pattern input DS280DF810EVM ,the CDR can't locked
Do you have idea about this issue ( PRBS15 Pattern as attached file)
2. Have any…
Part Number: DS280DF810 Hi,
We are considering DS280DF810 for QSFP28. The data rate is 28.050Gpbs. However, we can't find the register settings for common/standard data rates. Would you please provide the 28.050Gbps settings?
Would you please provide…