Hi,
After reading your threads, the radiation emission is coming from the BBB. I agreed ground the LCD may not help because it's not the source of radiation emission. It's hard to rule out and provide you an advice on BBB because we don't have experience…
Hi Leonardo,
You can regard this TxIN23 bit as an extra general-purpose bit. The reason why there are 28 input bits is because each LVDS pair, in OpenLDI fashion, serializes 7 bits per pair. Since a 24-bit application only requires a total of 27 bits…
Other Parts Discussed in Thread: DS90C385A Dear Sir
we confuse DS90C385A mapping question, from DS90C385A datasheet figure 3 mapping is different snla014 application note shows.
May you pls suggest us which one is correct?
For example,from DS TxIN0…
Other Parts Discussed in Thread: SN75LVDS83B , DS90C385A Hi,
Could you help make a comparison between DS90C385A & SN75LVDS83B? Which parameters are the key considerations when I'm choosing one for an application.
Thanks.
Part Number: DS90CF384A Other Parts Discussed in Thread: DS90CF386 , DS90C385A Hello team,
I am working on a new carrier board design based on the Compulab UCM-iMX8M-Plus System-on-Module (NXP i.MX8M Plus SoC). I am using the DS90CF384AMTDX/NOPB as…
Part Number: DS90C387A Other Parts Discussed in Thread: FLINK3V8BT-85 , DS90C385A Tool/software: Is there a evaluation kit for DS90C387A or similar? If so where can I buy 5?
Thanks,
Sunny
Part Number: DS90CF386 Other Parts Discussed in Thread: DS90C385A There is confirmation in the DS90CF386 and DS90C385A Specifications.
In DS90CF386 datasheet, Output SetupTime:Min 2ns @85MHz In DS90C385A datasheet, Input SetupTime:Min 2.5ns @85MHz…
Part Number: TIDA-010013 Other Parts Discussed in Thread: DS90C385A , Hello team,
could you please advise, if there are any limitation specs of LCD itself, that have to be taken into account,
if customer wants to use DS90C385A to implement RGB-to…