Part Number: DS90LV019 Tool/software: Hi
Please give me PSPICE model to MPN: DS90LV019.
I am not able to convert the IBIS model to PSPICE Model.
please help me for generating pspice model.
Thanks & Regards
Om Prakash Roy
Part Number: DS90LV019 Tool/software: Hi,
We are conducting an internal Failure Mode and Effects Analysis (FMEA) for our products and require specific information regarding the behavior of the following TI ICs under short and open conditions:
Target…
Part Number: DS90LV019 Hello,
My customer has unexpected outputs from D+/- as shown below. They expect LVDS signals, but these aren't.
Their current schematic is shown below. There 2 PCBs where PCB1 has FPGA and PCB2 does DS90LV019. These PCBs are…
Part Number: DS90LV019 Tool/software: Hi,
If only the receiver function of the DS90LV019TMTC is used, should the pins related to the transmission side be fixed to GND so that they do not become undefined? I think that pins 1, 2, 11, and 12 are the relevant…
Part Number: DS90LV019
Hi,
I have a RF Driver to be driven through an FPGA
Below are RF Driver parameters
Can i use DS90LV019 with output temination impdeance as 330 Ohm
If not kindly suggest a LVDS to TTL converter for above kind of inputs…
Part Number: DS90LV019 Hi, I would like to know the max allowable junction temperature and the various thermal resistance values (Junction-case, junction-board and junction-ambient) for DS90LV019TMTC/NOPB. Thank you. Best, Prathik
Part Number: DS90LV019 We are designing with the DS90LV019 LVDS Driver/Receiver.
We will be using the Driver section but have no need for the Receiver section.
So we will disable the Receiver section by connecting the RE(not) input to VCC.
In this…