Other Parts Discussed in Thread: DS90UB913A-CXEVM Please advise me using DS90UB193A-CXEVM
Q1. DS90UB913A-CXEVM is used in POC mode, supplying 5V CD from DS90UB914A how much current does DS90UB913AEVK consume at most?
Q2 How much current can POC supply…
hi Jiashow,
yes- i'm using PoC - see below block-diagram :
regard the schematics- i'm using MARS DS90UB954 adapter from "OnSemi"
After looking through the datasheets and schematics (of DS-954) I found that on RIN0+ & RIN0- the capacitors are…
Hi Erwin,
1) The video input pins of 925 are sampled once per clock cycle, so you can use however many of the 24 that you need. If you only need 12, that is fine. For the sync signals, these are limited to a certain number of transitions per PCLK cycles…
Part Number: DS90UB964-Q1 Hi Sirs,
We suffer a issue : UB964 cann't output
May you please help to give us some suggestion . thank you very much.
The architecture is as the following:
1. AR0144 (PCLK 74.25Mhz 12bits parallel mode) -> UB913 ->UB914…
Other Parts Discussed in Thread: DS90UB928Q , DS90UB925Q-Q1 , DS90UB928Q-Q1 Hi,everybody
I have a question about DS90UB914A and DS90UB928Q.
If signal to LVDS port(RIN & TXOUT) are disturbed by ESD,will LVDS IC reset?
Or are there any other conditions…
[ DS90UB914A-Q1 ] Not to use GPIO
Hi Expert, It seems that there are no pull-up/down resistors in GPIO[1:0] and GPIO[3:2] pins. If we don't use these pins, can these be left open? * No GPIO function used between 913A and 914A * No multiple camera frame…
Other Parts Discussed in Thread: DS90UB914A-Q1 Hello,
We are using the DS90UB913 and DS90UB914 pair to transmit data in 720p30fps mode (camera to MCU). During PCB assembly, there was a slight mixup and we have paired the DS90UB913A with the DS90UB914Q…
Hi Team,
Please advise me the question bellow:
Q1. How much Intra Pair Skew, does DS90UB914A tolerate at most? The definition of the Intra Pair Skew is that the time difference between positive and negative differential inputs to the device.
Q2…
Other Parts Discussed in Thread: DS90UB913A-CXEVM , DS90UB914A-CXEVM Hi team,
Please advise me on the following questions.
Q1. On page 59, Figure 46 shows the allowable loss curves and EQ gain curve. Can you explain why allowable loss curve of the…
Part Number: DS90UB914A-Q1 Hi Sirs,
We suffer a issue : UB914 cann't output
May you please help to give us some suggestion . thank you very much.
The architecture is as the following:
1. AR0144 (PCLK 74.25Mhz 12bits parallel mode) -> UB913 ->UB914…