Part Number: DS90UB933-Q1 Hi,
Are there any concerns in terms of meeting Serializer requirements (Trise, Tfall, etc) if we need to use SiT8924BAB73-18E-36.000000 or MC2016K36.0000C16EST ?
PCLK is 36MHz
Thanks,
Nandini
Part Number: DS90UB933-Q1 Other Parts Discussed in Thread: DS90UB913A-Q1 , How do I determine if the DS90UB933-Q1 or DS90UB913A-Q1 device is operating in RAW10, RAW12LF, or RAW12HF through registers?
Part Number: DS90UB933-Q1 Other Parts Discussed in Thread: DS90UA101-Q1 , DS90UA102-Q1 Hi team,
Hope you are doing well!
1. My customer said that UB933/934 is used on the market to implement I2S serialization and transmission, but I did not see such…
Part Number: DS90UB933-Q1 Dear,
How does DS90UB933 know the sensor bit width, RAW12 or RAW10?
I found that 0x05 register of DS90UB933 is used to configure 10bit or 12bit.
Does custom need to config this register before sensor image stream on…
Part Number: DS90UB933-Q1 Hi Team,
There is a good new that we DIN DS90UB913-Q1
And there have one thing need your support!
Customer is looking for the replacement of DS90UB913-Q1 (P2P would be better )
1.May I know the difference between DS90UB933…
Part Number: DS90UB933-Q1 Other Parts Discussed in Thread: DS90UB934-Q1 , hi team,
now customer will evaluate DS90UB933-Q1 and DS90UB934-Q1, they have some question about TI camera FPDLINK.
could you help support:
1 Communication capability meets…
Part Number: DS90UB933-Q1 Can we feed RAW 10 data from image sensor in DS90UB933 12 bit mode.
My calculated bandwidth from image sensor is 1.33 Gbps and want to feed in DS90UB933 using 12 bit mode, this is possible ?
Part Number: DS90UB933-Q1 1; When the contact discharge and air discharge test (4/6KV) is carried out on the screw position of the product, the image will flicker with probability. If the product extension wire is shortened, the probability will be reduced…
Part Number: DS90UB933-Q1 Hi Team,
Our customer is using the DS90UB933-Q1.
The System block as shown:
We have a question: instead of using a camera, the customer uses FPGA to convert DSI signal to Parallel signal.
After customer get this data…