Part Number: DS90UB933-Q1 hi Team
At present, it is found in the actual boarding test that the control screen will flash on the 360 look around interface (see Annex),
one At present, the frequency of PCLK is set to 95MHz, which is close to the limit…
Part Number: DS90UB933-Q1 Other Parts Discussed in Thread: DS90UB934-Q1 , hi Teams:
How can ds90ub933-q1 and ds90ub934-q1 output bt656 in BIST mode?
The following is the schematic diagram of ds90ub934-q1.
Ds90ub933-q1 uses ti's development board…
Part Number: DS90UB933-Q1 Hi team,
For 933 power up sequence, does the VDDIO & VDD18 rise time must be larger than 1ms? It seems too long.
935 and 953 doesn't need such long time.
BR
Jiawei
Part Number: DS90UB933-Q1 Other Parts Discussed in Thread: DS90UB662-Q1 , Hi Expert,
Could you please confirm whether ds90ub933 can work with ds90ub662 or not? From my understanding, it cannot. But in below e2e thread, it says ok. So I am confused about…
Part Number: DS90UB933-Q1 Other Parts Discussed in Thread: DS90UB913A-Q1 , Hi whom it concerns,
I would confirm both DS90UB933-Q1 and DS90UB913A-Q1 as below points
1. These parts electrocal and internal block are same,right?
2. The external connnection…
Part Number: DS90UB933-Q1 Hi Team,
There is currently a new project" BSIS application "!
Customer would like to use DS90UB913-Q1!
Could you share what deference between DS90UB933-Q1 vs DS90UB913-Q1?
I want to recommend products suitable for…
Part Number: DS90UB933-Q1
Hi teams,
My customer would like to use DS90UB933-Q1 as standard Ser Des because of the wide bandwidth.
Does this device support not video signal?
If does, if we use VSYNC and VSYNC, can we transmit 14bit signal as…
Part Number: DS90UB933-Q1 Other Parts Discussed in Thread: DS90UB934-Q1 We use DS90UB933-Q1 IC, and the input signal is BT656.(another box,receive IC is DS90UB934-Q1 )
BT656 has 8 bit input, but 933 has 10 or 12 bit input, how can I connect 8 bit to…
Part Number: DS90UB960-Q1 Tool/software: Hi,
The whole architecture is like:
As you can see, we would like to split DIN0 and DIN2~9 from DS90UB933.
DIN0 is error indication pin from camera sensor. We would like to redirect it to ECU GPIO pins…
Part Number: DS90UB933-Q1 Hi Team
As I know we can recommend replacing MAX96705 with a similar device DS90UB933-Q1 to serialize DVP signals and connect with 960,
Is there a corresponding product with similar development specifications and performance…