Hi Murat,
You're welcome. Either one would be suitable. They both have the same integrated AFE and use the same measurement algorithm; the main differences are in MCU peripherals, memory, footprint and price. Please see the MSP430FR6047 and MSP430FR6043…
Sure. You can use 200kHz with this board. Are you designing a gas meter? If so, I would recommend MSP430FR6043 and EVM430-FR6043.
Best regards,
Cash Hao
Hi soorej,
Using the ez-FET on the EXP430FR4133 to download program to the MSP430FR6043 chip is no problem (Just connected 3V3 GND RST TST), the cable is correct, but you need to check the pin of the FR6043 chip (including power supply, GND, or other…
Part Number: EVM430-FR6047 Other Parts Discussed in Thread: MSP430FR6047 , EVM430-FR6043 Hello,
I am trying to implement a system to measure flow rates in an open channel with channel widths up to 5 - 10m. I have the following questions:
1. Is it…
Part Number: MSP430FR6043 Other Parts Discussed in Thread: MSP430WARE ,
Tool/software: Code Composer Studio
Hello,
My hardware:
Custom board based on " EVM430-FR6043"
MSP430FR6043
CCS 10.1.0.00010
When I'm using the "timer_a_ex2_continousModeOperationWithCCR0Interrupt…
Hi Thomas,
Thomas Anderson said: 1. Is it possible to add an amplifier module to excite transducers with higher voltage without causing damage to the board? Does it need a relay or analog switch to prevent damage to the receiver circuit of IC? What…
Hello,
The EVM430-FR6043 can also be used for 1MHz and 2MHz transducers. Please see the TI Design below and note the hardware changes required in section 3.1.1.1.1. The maximum excitation frequency is 2.5MHz.
http://www.ti.com/tool/TIDM-02005
Also…
Hi Robert,
Please take a look at the MSP430 Ultrasonic & Rotary Flow sensing MCU page for details on TI's ultrasonic sensing MSP430 MCU offerings.
The MSP430FR6043 and MSP430FR6047 microcontrollers (and their variants) offer solutions for applications…
1. We have not tested with both transducers on one side. The signal level will be lower this way, but you would have the possibility for a wider dynamic range since the path traveled through the medium is longer. For some customers, this may be an easier…