Part Number: LDC507X-SENSOR-DESIGN-TOOL Other Parts Discussed in Thread: LDC0851 Hello,
Our customer want a 2500 rmp, Pole pair 150, support clockwise and reverse sensor.
Could you please recommend a small size sensor.
Thanks,
Yuhao
Part Number: LDC507X-SENSOR-DESIGN-TOOL Hello,
I was wondering if there is a possibility of making a quarter cut version of the same Angular Co-Axial example sensor provided with the EVM board. We are dealing with some size constraints and are wondering…
Part Number: LDC507X-SENSOR-DESIGN-TOOL I am trying to create a custom design using the LDC5072 Sensor Designer and any time I try pressing the ‘Design Sensor’ button, the design will not be created. I believe it stops after not being able to open the…
Part Number: LDC5072-Q1 Tool/software: I have several questions regarding the use of the LDC5072 tool:
Under the "Sensor Type" section, there are multiple options like Angular Coaxial Type I , Angular Off-Axis , and others. Could someone please…
Part Number: LDC5071-Q1 Tool/software: Hello,
I am hoping to use the LDC5071-Q1 with a custom linear inductive sensor to give me absolute position of a linear slide.
I have been playing around with the LDC5072 Sensor Designer Tool and looking at the…
Christian,
For your design to work, you would need to set the ratio to 1 to generate the off axis coil. This will not generate the correct target for you though. In order to have a 5 pole target, you should set the tool back to angular co-axial and…
Phillip,
I was able to create a custom design using the Custom Sensor tab. The starting point was to create a design from the Mechanical Design tab, and then save the design. The next step was to transition to the Custom Sensor tab and modify the input…
Part Number: I2C-DESIGNER Tool/software: Unable to access "I2C designer tool" Referring below link I2C-DESIGNER Design tool | TI.com Please help to get access
Part Number: OPT4048
Tool/software:
Hi Team,
Can OPT4048 meet the following requirements?
When used on AR glasses, it is required to detect distances of more than 1m and a FOV of ±10 or 30 degrees
Are there any recommended designs for convex…