Other Parts Discussed in Thread: LM22670 Hi,
I have an application where I use the LM22670 as voltage inverter LM22670 Evaluation Board Inverting Topology and Application Notes (Rev. D) .
Now I want to synchronize it through the SYNC pin. The above…
Hello,
I want to fix a +12V potential in the output with a +24V input.
My problem: When the output current is higher than 600mA (with a charge of 20R), the voltage falls progressively.
All the capacitors are low ESR, and dimensioned by the datasheet…
Part Number: MSP430F4152 Tool/software: Code Composer Studio Hi,
We are now creating a new project of brushless motor (called BLDC below) control using MSP430F4152 as the MCU.
I use the following function to change the main clock of the system to…
Part Number: MSP430F4152 Tool/software: Code Composer Studio Hi,
We are now creating a new project of brushless motor (called BLDC below) control using MSP430F4152 as the MCU.
I use the following function to change the main clock of the system to…
Part Number: MSP432P401R Tool/software: Code Composer Studio Hi,
There are two troubles I met these days.
One is MCLK and the other is UART communication.
I download the same code on both EVM and the PCB we created.
EVM can work but PCB can…