Part Number: LM5012 Other Parts Discussed in Thread: LM5013 Hi,
I want to Turn ON and Turn OFF my Buck converter (LM5012DDAR) using EN/UVLO pin voltage.
May I know what is the minimum time required to switch the IC function from standby mode…
Part Number: LM5012 Other Parts Discussed in Thread: LM5013 Hi team,
My customer designed a circuit that Vin=48V, Vo=24V, Io=2.5A. And Vo stays normal of 24V when with no load.
But Vo will drop to 18V when increasing the load to 2A. Below is the SW…
Part Number: LM5012-Q1 Hi TI Team,
With reference to the above subject. We are using 100V BCK IC " LM5013QDDARQ1" & "LM5012QDDARQ1" in our IOT Telematic Device.
We did a hot plug test in the 100V BCK IC, during the Test when it reaches 75V the…
Part Number: LM5012-Q1 Hi ,
This is regarding MPN - LM5012QDDARQ1. I have some doubt for requirements of Input - (44V-52V), Output - 12V, 1A Ambient -(-40-125degC), Switching Frequency - 400KHz
1. I want to know if I select the switching frequency…
Part Number: TCAN2451-Q1 Other Parts Discussed in Thread: LM5012 , Tool/software: We are using the F28P65 series microcontroller for our 48V BMS and LM5012 IC. When the MCU enters HALT mode (requirement of sleep mode current of BMS), the total current…
Part Number: LM5013 Other Parts Discussed in Thread: LM5012 , Tool/software: Hello,
This post is regarding the input and output buck regulator loops' suggested in the datasheet of LM5013/LM5012 in section 9.4. As I understand the loops are as below…
Part Number: LMR38020-Q1 Other Parts Discussed in Thread: LM5012 , LMR38020 Tool/software: IC shows Iq current of 40uA at No load. At low load current (<1mA) as well as all at full load operating current will it maintain same? Or it's Iq active current…
Part Number: LM5164 Other Parts Discussed in Thread: LM5013 , LM5012 , , LMR38020 , LMR38015
Hello team,
Which devices has the best EMI performance, the LM5012, LM5013, LM5164 and LMR38020 xy?
Can you share the results of the EMI test of the best…
Other Parts Discussed in Thread: LM5012 , LM5013 Hello, I'm searchimg for an Buck-Converter. I have an Applicationwith following parameters: Input Voltage: Will be between 20V- 96V Output Voltage: 5V. Current: 1.5A at 5V - Peak will be around 2,5A. Important…
Part Number: TPS54260-EP Other Parts Discussed in Thread: LM5012 , LM5013 TPS54260-EP Buck Converter maximum input voltage range is 65V.
In our design, TPS54260-EP placed after TVS diode.
While performing lightning test , will get around 90V after…