Part Number: LP-CC1312R7 Tool/software: Hi,
With the release of the simplelink SDK 8.30.00.121, is it still necessary to patch the is_net_stack_up function for the router node with wfantund to work?
I may be doing something wrong, but the ns_node…
Part Number: LP-CC1312R7 Other Parts Discussed in Thread: CC1352R Tool/software: Hi, Very new to WiSUN and Contiki, I am wondering If it is possible to build communication on two different devices one running on WiSUN and other running Contiki, Assuming…
Part Number: LP-CC1312R7 Other Parts Discussed in Thread: CC1312R7 Hello,
The SDK example mcuboot_LP_cc1312r7 and mcuboot_blinky_LP_cc1312r7 of LP-CC1312r7 can be compiled and successfully burned to display running lights.
However, configure the serial…
Faruk Sozuer said: When I look at the forum, it is mentioned that IEEE802.15 mode is HSM. Does this apply to the CC1312R7?
High Speed mode(HSM) is not available on CC1312R7. It is only on the CC13x0 device.
Part Number: LP-CC1312R7 Tool/software:
I'm having problems making the mlx90614 sensor give acknowledgement while using the LP-CC1312R7 launchpad with SIMPLELINK CC13XX CC26XX SDK. Two weeks trying to get ACK but the code i wrote cannot do it. I will…
Part Number: LP-CC1312R7 Other Parts Discussed in Thread: CC1312R7 Tool/software: I am looking for an RF transceiver capable of transmitting and receiving PWM signals at 5.8 GHz. As someone new to RF technology, I don't have a deep understanding of its…
Part Number: LP-CC1312R7 Tool/software: Hello, I´m using the provided NVS driver to control data write to the included but I have checked that this driver fails to write the data in the correct positions in the MX25R8035F chip. I configure and work as…
Part Number: LP-CC1312R7 Other Parts Discussed in Thread: SYSCONFIG Hello,
I´m using the NVS with the MX25R8035F flash, which works completely fine.
Now I want to use the same SPI bus to control another peripheral (a SPI LAN controller), this has…
Part Number: LP-CC1312R7 Hello,
I´m working in a project when sometimes the target device disconnects from the JTAG and outputs the next error message:
Cortex_M4_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the…
Part Number: LP-CC1312R7 Other Parts Discussed in Thread: CC1312R7 , UNIFLASH Tool/software: Hello,
I'm in the implementation phase of designing and implementing a bootloader uploader for the CC1312R7, this program has worked well in the past but sometimes…