Other Parts Discussed in Thread: LP8556 Hi,
We wanted to know the maximum current and out put voltage rating for LP8556TME-E09. As per datasheet, the max LED current per string is 25mA and output voltage is 16V to 34.5V but feature list says it can…
Hi Nidhi,
For ALSO pin, just leave this pin alone is ok. What's your detail application? We have some other backlight driver:
For 6 channel, you can choose :LP8556, TPS61177A, TPS61187
For 8 channel, you can choose :TPS61196, TPS61199
Regards …
Hi Brian,
I'm sorry for the late response. As the datasheet says: "Writing to EEPROM Control register of production devices is not recommended. ". That means it's not suggest for customer to use a MCU adjust setting in EEPROM. But you can connect sales…
Hi Andy,
We have plenty choices meeting your requirement, please take a look at LP8556, TPS61176, TPS61177A.
Could you please share more information about who is the customer, what is the end equipment? We could help to you to decide which one it the…
Chaitanya,
The best one we have is the LM3532 with the ambient light sensor input. This can only get up to 30mA per channel. We do have others that have more current (LP8556), but no ALS.
Thanks
Travis
Part Number: AM5718 Hardware: custom carrier board + TQMa5718 custom module from TQ-GROUP
Software: PROCESSOR-SDK-LINUX-AM57X 06_03_00_106
When we activate either PRU1, PRU2 or both of them in the dts file (see attached file "am571x-art57xx_precomp_prus2…