Part Number: TDA4VM Hi experts,
I am using PSDKRA & PSDKLA V7.0 on EVM borad to test the vision_apps and one of the apps "run_app_stereo.sh" can't exit when i enter "x".
Could you double check this function on your side? The serial log show below…
Hi Wyatt
Thanks for your help.
The battery is Samsung INR18650-25R(2500mAh) CHEM ID:2068
202305121740.gg.csv
4-series battery pack, the maximum charging current is 2.5A, the rated output power is 100W, and the charger voltage is initially fixed…
Other Parts Discussed in Thread: WL1837 I've been working on this for a few months now. I'm using a wl1837 chip on a DART-MX6 board and transmitting 5GHz Wi-Fi over channel 48. I have attached the output of ANT1 directly to a spectrum analyzer via a 10…
Hi Ali
Thanks for the reply.
1. I am using ISO1050EVM CAN transciever.It has 120 ohm terminating resistance.Here is the datasheet:
user guide.pdf
ISO1050.pdf
2.I am using oscilloscope to observe the waveforms-CANH/CANL/TXD pins and all.…
About
ALE stands for Address Lookup Engine and it is a module inside CPSW 5G/9G module which is used to implement features specified in IEEE 802.1 Q protocol like VLAN tagging, Learning, Forwarding, Filtering, Rate control, Mirroring etc. (A full list…
Hi Bin:
I configured USB according to what is explained in the videos.
I dont see any usb error messages during linux startup.
After "modprobe g_ether", directory "/sys/class/udc" is empty,
and "lsmod" shows "g_ether" and other usb related modules…
Other Parts Discussed in Thread: AM5718 , DRA722 , PMP , TLC59108 , TMP102 , AM5728 Tool/software: Linux Hi,
We have developed a custom board with AM5718 processor and we are using ti-processor-sdk-linux-am57xx-evm-02.00.01.07. I am using eMMC boot…
HI Titus S.
I dont have any idea of "matrix gui" .
Now I am using 4.10 I get the below log.
root@beagleboard:~# lsmod
Module Size Used by
bufferclass_ti 6612 0
pvrsrvkm 521032 1 bufferclass_ti
drm 242585 1 pvrsrvkm
omapfb 39055 2
cfbfillrect…
Part Number: BQ76952
We are trying to control the DDSG and DCHG outputs that are driving the low-side FET driver circuit in our design. Unfortunatly we can't make it work. We assume that it could be caused by a proper register setting of the BQ76952…