Hi Ryan,
so i saw the code from the MSP-EXP430G2_I2CMSPBootHost Project and i have a question about the target application .txt data.
The Demo Host project uses the application like "App1_G2553_I2C_BSLBased_G2Host.txt" to flash via I2C/UART/SPI to…
Hi,
Attached are the Boosterpack Pinout and MSP430F5529LP User guide. Please see Figures 40 & 41 in User Guide for Launchpad Pinouts. The unused lines (GPIOs) on the P2 & P3 of the BOOSTXL-CC1120-90 can be used for your Keypad.
If you change the Pins…
Go here:
http://processors.wiki.ti.com/index.php/MSP430_LaunchPad_%28MSP-EXP430G2%29?DCMP=launchpad&HQS=Other+OT+LaunchPadWiki
And look for these references:
LaunchPad Documentation
Quick Start Guide for LaunchPad | Download Now
User…
You will probably find all of your desires impossible to meet. I think the lack of a good low cost fairly universal programmer that works for most of TI's current and future devices is an unfortunate situation, especially because there are several unique…
Part Number: PGA460 Other Parts Discussed in Thread: USB2ANY , , ENERGIA , , PGA450-Q1 , PGA450Q1EVM
Ultrasonic Time-of-Flight Measurements (through Air)
If your application requires the use of ultrasonic time-of-flight to measure distance through…
Hi Danish,
The following is install.log:
01/24/2017 18:01:27(GMT) - Util::checkurl - Checking software-dl.ti.com/.../timestamp.txt from checkurl
01/24/2017 18:01:27(GMT) - formatUrlForDownload - external url software-dl.ti.com/.../CCS7.0.0.00043_osx…
Hi,
I have tried your code. You are right. Free run mode will cause the target device does not resume code execution after LPMx.5 wakeup.
You can find the answer after you look through this document from page 64 to page 66. Code Composer Studio™ IDE…
Hi Muller,
You can use the Graphics_drawString or Graphics_drawStringCentered functions, this is shown in the MSP-EXP430G2_Grlib_Example provided with the MSP-GRLIB package in Resource Explorer. However you will need to first convert your received…
Actually, I've just found the installation log for CCS v8.
Here it is.
06/05/2019 04:22:34(GMT) - ProgressBar::Run - RunSysInfo /tmp/ccs_b2a7c8fa-e785-4660-64fa-230dd5a8bf3c/install_logs/20190605132231/ccs_setup_8.3.0.00009_install.log ::progressBar0…