Given that you are using 8 MHz crystal and interested in SMCLK, Leo is right.
At one of your 2 MSP430F1612, you can connect the 8 MHz crystal to XT2IN and XT2OUT to generate SMCLK (and optionally also MCLK but not ACLK).
You can set up one of the…
Other Parts Discussed in Thread: MSP430F2617 , MSP430F1612 I'm considering the MSP430F2617 as a footprint compatible upgrade to the MSP430F1612. Can you tell me which peripheral modules differ between the two?
Other Parts Discussed in Thread: MSP430F1612 Hello,
For MSP430F1612, for DAC12 I cannot enter the value in DAC12_0DAT. Below is the code and also the screenshot of IAR. As you see, no data loaded in DAC12_0DAT, neither voltage on P6.6/DAC0 processor…
Other Parts Discussed in Thread: MSP430F1612 Hello,
I have MSP430F1612 with RS232 transceiver connected to USART0. For testing and learning purposes, I use Hyper terminal to communicate with PC in idle-line mode. When transmitting to PC, everything…
Other Parts Discussed in Thread: MSP430F4132 , MSP430F1612 Hello,
I am working on a project with MSP430F4132 and the datasheet specifies that maximum crystal oscillator frequency is 6MHz. Incidentally I bought the Launchpad EVM that has an MSP430F1612…
Other Parts Discussed in Thread: MSPMATHLIB , MSP430F1612 , MSP430G2553 Compiling for an MSP430F1612 target, I am receiving remark 10422 (ULP6.2) recommending the use of MSPMATHLIB (libmath.a). However from what I can tell there is no version of libmath…
I've been working a project using DRV8821EVM (Dual Stepper Driver) as a test bed for some time now. Very successful to this point.
BUT, I now need more program (memory) flash than the MSP430F1612 provides. I am OK with changing the part out on the EVM…
MT7316,
XT1 is not a source for SMCLK for the MSP430F161x, MSP430F16x, and MSP430F15x devices.
The LFXT1 oscillator replaces XT2CLK only on MSP430x11xx and MSP430x12xx devices.
This is noted on page 112 Section 4-3 of the MSP430x1xx User's Guide…
Other Parts Discussed in Thread: MSP430F1612 , TUSB3410 Hello,
does anyone know how to reprogram the MSP430F1612 mounted on the LaunchPad development
board ? That component has the debugger software programmed and maybe there are some
memory security…
Other Parts Discussed in Thread: MAX3221 , MSP430F1612 , MSP430F149 hi guys...
i want to connect my msp430f1612 with max3221 to see the output on the hyperterminal but i couldnt see any out put on the hyperterminal.even the result on the oscilloscope…