Hi guys I'm trying to do this question for an assignment using the msp430 -ez430-f2013 but the value at the memory address I'm moving to stays at 0xFFFFh.The code I'm using seems correct(at the bottom of this post). Is there something I'm missing ?
…
The SD16 and SD16_A can be configured to randomly generate bytes, providing a high quality source of entropy as well as doing its usual job as an ADC. An application note about this is attached.
In the note I need to estimate the minimum amount of contact…
Hello
I'm completely new using IAR embedded workbench,
I'm trying to develop the codes to implement in the master and slave MCU units
the MCU master has simply to activate each slave, on at a time, with a certain time interval between each activation…
Other Parts Discussed in Thread: MSP430G2553 Hello, Im begginer with microcontrollers an Im having troubles with serial comunication with a pololu maestro servocontroller, I got serial comunnication with an arduino board an it was easy but with the msp430…
Other Parts Discussed in Thread: MSP430G2452
hi
i am joju mohan i have problem with uart rx section my cod is given below . In this tx from mcu is happening but rx is not working
This is a program for eco rx byte at rate 9600 for launch pad so…
Other Parts Discussed in Thread: ENERGIA , MSP430G2452 energia program for interfacing 4*4 matrix keypad ..
if some one have please send me at patel_parth15@live.com..
and tell me how to include #include <IRremote.h> and #include <keypad.h>
and…
hi
i am new to msp430 mcu when i used i2c library function i got 3 errors
1 [E0002] Illegal mnemonic specified
2 [E0003] Only labels and comments may begin in the first column. Make sure that the label name is not a reserved keyword.
3…
Other Parts Discussed in Thread: BQ24650 Hello,
I am looking to implement a 4V solar charged LiFePO4 to drive a 350mA portable LED light. I would like to implement it with the MPS430, the BQ24650, and a BQ24710 gauge, all to the appropriate driver for…