Part Number: MSP430F47187 Tool/software: Hiii sir,
I am curious to know about which flash controllers are used in embedded flash controllers?? is it nand based or nor based flash controllers ??
and if they are using nor based embedded flash controllers…
Part Number: MSP430F47187 Tool/software: Hi Team, 1. With what sampling rate the 16-bit ADCs are working in this MCU?
2. UP tp what harmonic this MCU can calculate accoridngly?
Regards,
Maryam
Part Number: MSP430F47187 Tool/software: As i understood its a low-power micro controller which works on 32.768 kHz,
Can i configure the Clock initialization using 8MHz.
What will be the DCO / MCLK / SMCLK
Also ADC SD16A to be of 1ms interrupt…
Part Number: MSP430F47187 Other Parts Discussed in Thread: ADS1115 , MSP430WARE Tool/software: Is it possible for interfacing such IC(ADS1115) with MSP430F47187 to collect adc sample of 4 Channels as fast as possible.
Can i get a sample code for the…
Part Number: MSP430F47187 Dear Team,
My name is Sandip, and I am reaching out to you regarding a recent purchase we made with your company from the Alibaba website. We have encountered some concerns with the product's originality, and we seek your assistance…
Part Number: MSP430F47187 In Code Composer Studio ( Version: 5.5.0.00077 ) "#24011-D argument to option -v (version) is out of range" I get an error saying I don't know how to deal with it, so please let me know.
Part Number: MSP430F47187 Heloo.
Because I am not familiar with English, the sentences may be strange.
The interrupt cycle of DMA created from SD16A changed at low temperature (below -5°C) on MSP430F47187. The amount of change depends on the temperature…
Part Number: MSP430F47187 Helllo Everyone,
i am using MSP430F47187 for our development. i have calculated voltage and current samples ,from these samples ,i have calculated RMS voltage,RMS current ,powers and power factor but these powers are in absolute…
Part Number: MSP430F47187 I have to initilize ALCD , my code is
LCDACTL = LCDACTL_INIT; LCDAPCTL0 = LCDAPCTL0_INIT; LCDAVCTL0 = LCDAVCTL0_INIT; LCDAVCTL1 = LCDAVCTL1_INIT;
and when in off mode the lcd is disable
LCDACTL = LCDAPCTL0 = LCDAPCTL1 …
Part Number: MSP430F47187 Other Parts Discussed in Thread: TPS54060 Hi Team,
hope everyone doing well!
we are using MSP430F47187 in our circuit . our circuit consists of capacitive power supply as well as coin cell battery option .
Problem: when…