Part Number: MSP430FR2153 Hello guys,
This is Ezra. I am currently working on a project that requires a significant amount of flash memory and RAM (greater than 64 KB FRAM and greater than 8 KB RAM). To manage this, I have divided the work between two…
Part Number: MSP430FR2153 Other Parts Discussed in Thread: MSP-FET Tool/software: I've got a system issue that I'm trying to debug, but having issues figuring out how it's getting into the state in which we see the failure. I have an interrupt, set to…
Part Number: MSP430FR2153 Other Parts Discussed in Thread: MSP-FET , UNIFLASH Hello,
I'm trying to program my microcontroler MSP430FR2153 with a MSP-FET Flash Emulation Tool.
The micro is powered by 2V3 and, in order to use the debug mode, I connected…
Part Number: MSP430FR2153 Hi,
Doc SLAU445I - MSP430FR4xx and MSP430FR2xx family User's Guide, Table 21-8. ADCMCTL0 Register Description, says that I can set ADCSREFx to 000b = {VR+ = AVCC and VR– = AVSS }, and this will use "AVCC" as the ADC reference…
Part Number: MSP430FR2153 Hi,
The documents and driverlib code seem to conflict a little of ADC clock source options.
Document SLAU445I MSP430FR4xx and MSP430FR2xx family User's Guide
Figure 21-1. ADC Block Diagram shows ADCSHSx selects clock sources…
Part Number: MSP430FR2153 Team,
One of our customers is using MSP430FR2153 device. They want to use window comparator mode for only one channel. But when they configured it, all the channels are are going through the window comparator mode and generating…
Part Number: MSP430FR2153 How to use window comparator function in order to create interrupt using MSP430fr2153BL. If anyone has used this function, please support me in this issue.
Part Number: MSP430FR2153 Hi,
I could see that pin P1.1 supports both ADC input and analog comparator input as well. I want to use the same input pin for ADC and eCOMP module simultaneously. The input should go to both modules simultaneously. From the…
Bryce Nesbitt said: Am I correct that the bootloader does not use UCA0 nor UCA1, but rather two random I/O ports? The MSP430FR2153 datasheet SLASEC4D has:
Where:
The UART BSL pins are for UCA0TXD / UCA0RXD
The I2C BSL pins are for UCB0SDA /…