Hi,
unfortunately we can only hope that the address is not already used. Otherwise we have to implement a custom BSL with SPI bus. But I know that there is not a SW available from TI for this, and it is a hard work for us.
Hi,
the input of ADC is a a 0-3V signal.
The ref of the ADC is internally set at 2V and the AVCC of the uC is 2.7V.
1) because Vin > AVCC, is an input protection needed in order to avoid damages? Is e series resistor enough?
2) If Vin > Vref…
Part Number: MSP430FR6879 I am using my msp430fr6879 in slave mode to talk to a different circuit which is acting as master ,
It works fine if I switch on the master only after the switch on the slave .
but if I power up my master first and then the…
When it comes to SPI, just send two 8bit bytes. SPI don't care that there is a pause between bytes (or pause between bits even) as it's the CLK that is in charge.
USCI is buffered so there will not even be a pause between the bytes as long you feed…
Part Number: MSP430FR2033 Other Parts Discussed in Thread: MSP430FR6879 , MSP-FET Hi,
I'm working on a product that contains a main board (using MSP430FR6879) and a daughter-board (using MSP430FR2033). The two boards communicate over SPI.
When doing…
Part Number: MSP-GANG Other Parts Discussed in Thread: MSP430FR5969 , MSP430FR6989 , MSP430FR6879 Tool/software: Hello all,
I have a problem with two different GANG's: old with version 1,04 and new with version 1,05. With GANG's I want to download code…
Part Number: MSP-GANG Other Parts Discussed in Thread: MSP430FR6879 I have MSP-GANG programmer. I connect one PCB with MSP430FR6879 and program in ‘interactive’ mode with PC through JTAG. Is OK.
When I switch in addition second channel, GANG returned…
Hello,
na na78 said: Can you explain each operation?
See:
https://e2e.ti.com/support/tools/ccs/f/81/t/411164
http://www.ti.com/lit/ug/slau367o/slau367o.pdf
http://processors.wiki.ti.com/index.php/Debug_Handbook_for_CCS#MSP430_2
https://e2e…
Part Number: CC3220MODA Hi
This thread is related to following. e2e.ti.com/.../806220 I splitted question to be simple to understand.
The customer faced a problem that MSP430FR6879 firmware download by OTA is failed. SDK version is 2.30.0.05.
Following…
Hi Winter,
Thank you for responding to my question.
I got the following question from my customer. Would you please investigate this additionally?
Does this problem of ESD noise have the type that consumption current continues to increase in MSP430…