Part Number: MSP432P4111
Hi,
We have bought some units of MSP432P4111IPZR (TQFP-100) for our design. We have designed a 4-layer board for use with TI MSP432.
I followed the datasheet specs, but unfortunately, some seconds after the power-up…
Part Number: MSP432P4111
Hi,
I have been trying to debug a custom MSP432P4111 board using a Launchpad as debugger through JTAG (10-pin) connector. I have been facing the following message when I run the debugger in CCS: "Error connecting to the…
Part Number: MSP432P4111 Tool/software: Code Composer Studio I am using the code below to check analog inputs AI0 and AI1 on the ADC module, and when I apply a DC signal to both inputs A0 does not change in value while A1 tracks the voltage correctly…
Hello Jesu,
I came to the same conclusion. The protocol that is used wraps the payload with a header-footer, where the header has the size of the payload, so I'll just continue with the approach where I always wait for the exact amount of data. I wont…
Part Number: MSP432P4111
Hi,
I'm opening this thread because I clicked "This resolved my issue" by mistake in another thread ( https://e2e.ti.com/support/microcontrollers/msp430/f/166/p/814349/3014097#3014097 . Unfortunately, this forum does not…
I have gone back in the lab and confirmed with the example that the average current consumption is around 650uA and that it increases to about 950uA when the ADC is active.
Specific to your question about the ultra-low power, I think the issue is that…
Part Number: MSP432P4111 Hello All,
I have a query regarding the Debugger to be used for MSP432P4111 controller.
I have a PCB designed with this controller. Now I want to understand the Debugger to be used for this controller.
In the controller…
Part Number: MSP432P4111 I use the version of simplelink_msp432p4_sdk_1_50_00_12 to build my software, I use the pin P9.6 as uart RXD ,but it did not recevive any data . so I want to ask whether the uart function of P9.6 is available .
Part Number: MSP432P401V Other Parts Discussed in Thread: MSP432WARE Hi Team 432,
Some questions WRT P401 & P4111..WRT TI Drivers.. Driver_Lib.. Flash APIs.. SDK format/structure.. 432 sampe code/projects..
1. Seems the 432 SDK has changed a bit in…