Part Number: MSPM0C1106 Other Parts Discussed in Thread: MSPM0H3216 , MSPM0G3507 Tool/software: Hello,
I’m developing on the MSPM0C1106 (Arm Cortex-M0+, 64KB Flash / 8KB RAM) and would like to run FreeRTOS on this device.
This makes me wonder whether…
Part Number: MSPM0C1106-Q1 Other Parts Discussed in Thread: MSPM0C1106 Tool/software: We have a use case where our controller MSPM0C1106 will be reading 7 sensors using SPI interface and the sensors will be daisy chained and use same Chip-select.
Can…
Part Number: MSPM0C1106 Tool/software: Hi team,
I’d like to develop using the MSPM0C1106 and CCS Theia. I installed the MSPM0 SDK and CCS Theia, and CCS Theia successfully discovers the SDK under Products . However, when I try to import an example project…
Part Number: MSPM0C1106
Tool/software:
Hi Expert
Customer need to redefine fputc function but the compiler reports the redefine issue below:
I searched the e2e thread, there is one post mentioned that putchar should not be called to avoid the…
Part Number: MSPM0C1106 Tool/software: Hi, experts:
I'm working on mspm0c1106 evk and CCS 20.3.0, create a empty project and set TIMA0 for PWM_0, use MCU package as VQFN-24(RGE), finding PA3&PA4 can't turn on led, attached is the project I created,…
Part Number: MSPM0C1106 Tool/software: Hi Expert
Customer want to disable multiple IQRs at a time with one API, but seems our drivelib only has NVIC_DisableIRQ() to disable one IRQ at a time, does drivelib has other function to meet this need?
Thanks…
Part Number: MSPM0C1106 Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hi Expert
Could you please help to guide me how to configure the IWDT in sysconfig? I look into the SDK IWDT demo code, I cannot find where to configure this spec, but…
Part Number: MSPM0C1106 Tool/software: Hi Expert
I use CCS20.2 and mspm0_sdk_2_05_01_00 for MSPM0C1106 debug, if I enable the Arm hex utility and select intel hex, the debug folder will generate .i1/ .i2/ .i3 file and output window will output warning…
Part Number: MSPM0C1106 Tool/software: Hi Expert
I see in datasheet PA0 and PA1 are ODIO (5Vtol)with wake structure, does that mean it must pulled up with external VCC for generate high output? or it can out put 3.3V by itself?
Thanks
Joe