Part Number: OMAPL138B-EP Hi.
I have OMAP LCDK kit. I want to transfer data from MATLAB in PC to the LCDK EVM kit through USB serial.
Is there any tutorial for doing the above?
Regards ,
Sagnik Basu.
Part Number: OMAPL138B-EP Other Parts Discussed in Thread: OMAP-L132 Tool/software: Code Composer Studio Hi:
I met some problems when using OMAP-L132.
1.The power-supply timming: TI recommended in the order of 1.2V - 1.8V - 3.3V . If i change the…
Part Number: OMAPL138B-EP Tool/software: TI C/C++ Compiler Dear all,
we are using the OMAP L138 ARM + DSP Controller. We have SYS/BIOS and NDK running on the ARM, no operating System on the DSP.
We had a bug in the DSP firmware with an instruction…
Part Number: OMAPL138B-EP Other Parts Discussed in Thread: OMAPL138 Tool/software: TI-RTOS As per omapl138 Datasheet Page 24 the following memory map can only used for NAND EMIFA async data (CS2) 32 MB EMIFA async data (CS3) 32 MB EMIFA async data (CS4…
Part Number: OMAPL138B-EP Other Parts Discussed in Thread: SYSBIOS
Tool/software: Code Composer Studio
Hi Champs,
since switching from CCSv5 to CCSv6 I can't edit/view the platform file using the RTSC tools/platform/edit/view menu anymore. Is there…
Part Number: OMAPL138B-EP Tool/software: TI-RTOS I am developing application on OMAP L138 processor using EDMA, my OS is SYS/BIOS 6.45. I have met problem with trigger of interrupt of EDMA, when it's running, interrupt is happen approximately 20-30 times…
Part Number: OMAPL138B-EP Tool/software: TI C/C++ Compiler Dear all,
I am working on C67xx project (OMAP L138 DSP, CCS 5, Compiler 7.4.20). Further, we are using -O3, --opt-for-space=3, --opt-for-size=2, and --optimize-with-debug=on.
I compiled with…
Part Number: OMAPL138B-EP Tool/software: Code Composer Studio Dear all,
I am referring to the C6000 compiler in CCS 5.1.1. We are using -O3 -ms3
The compiler seems to refuse inlining of functions involving struct or volatile parameters. This is also…
Part Number: OMAPL138B-EP Other Parts Discussed in Thread: OMAPL138 , OMAP-L138 Tool/software: Starterware Why My Board Not Erased ?
D:\Work\OMAPL138_StarterWare_1_10_04_01_21092017Work\ARMDSPTestWit Change_300Mhz>sfh_OMAP-L138.exe -targettype OMAPL138_LCDK…
Part Number: OMAPL138B-EP Other Parts Discussed in Thread: OMAPL138 Hi,
I have been given a project recently related to communication systems. The board that we have decided to develop the project is LCDK OMAPL138. In this project we need both ARM and…