Part Number: PROCESSOR-SDK-AM62X Tool/software: Hi Expert,
Does TI Linux SDK support cybersecurity?
Is there any document that states something about cybersecurity certification?
Thanks
Daniel
Part Number: PROCESSOR-SDK-AM62X
Tool/software:
Dear support:
Now I have encountered the operation optimization problem of the AM62x M4F kernel program, I would like to ask for advice。
(1)The test found that the program running on the M4F core…
Hi Wang,
W Z said: Could you please let me know the right steps to rebuild the RTOS libs?
You can build the makefiles present in the following folders using the make -f command.
1./source/kernel/nortos
2.source/kernel/freertos
Regards,
Nihar…
Part Number: PROCESSOR-SDK-AM62X Tool/software: Hi,
We are working in vxWorks with TI AM62x to make the changes w.r.t the errata:
2.3.1.3. PLL Programing Sequence Update To Avoid PLL Instability ( software-dl.ti.com/.../Release_Specific_Migration_Guide…
Part Number: PROCESSOR-SDK-AM62X Tool/software: Hello Team,
MCAL Package: MCAL_SitaraMPU_09.01.00
As per SWS_Mcu_00134, The MCU module shall provide at least the values MCU_POWER_ON_RESET and MCU_RESET_UNDEFINED for the enumeration Mcu_ResetType.…
haibin xiao said: 4,M4F core crash;
Can you please tell when the M4F crash, what error message do you see on console?
Also are you able to halt the core when issue happens?
Which example are you trying to run?
Part Number: PROCESSOR-SDK-AM62X Tool/software: Hello TI expert,
I imported the example into CCS, but I do not know how to make it run.
Should just take it as R5 core app?
Part Number: PROCESSOR-SDK-AM62X Tool/software:
Hi,
While browsing PROCESSOR-SDK-AM62X Software development kit (SDK) | TI.com
The latest mcu_plus_sdk is version 11_01_00_16 while the version I can download from ti.com/secureresources/AM62X-RESTRICTED…
Part Number: PROCESSOR-SDK-AM62X Tool/software: Hi,
I am using the TIMEOUT register to get time-delimited messages on ECU. as per TRM 1 unit of the register value is 1 baud cycle. but when I calculate as per each bit time I observing erroneous timeout…
Part Number: PROCESSOR-SDK-AM62X Tool/software: I need to debug the miniPCIE. The required functions include USB, UART, and SPI. Among them, USB and UART need to utilize the 4G function, while SPI needs to use the LoRa function.How should I configure…