Part Number: LP-AM243 Tool/software: Hi Poyra.
Our Situation:
Hardware is fully ready.
Software remains unsolved , blocking deployment.
We require 2 Digital Inputs and 2 Digital Outputs , mapped to EtherNet/IP and accessible via CODESYS…
Part Number: ADS1299-4 Tool/software: Hello TI's Engineer. I would like to make a design review of the ADS1299-4 schematic for my customer.
Could you please let me know the way to send the design (private design data) to TI's engineer email?
Thank…
Part Number: BQ25798 Tool/software: Hello, Please review the schematic and share your feedback. I have a question regarding the system voltage, When VBUS is present at the input, is the system voltage (VSYS) directly equal to VBUS, or does it depend on…
Part Number: LM5050-2 Tool/software: Hi Team
Can you help to review the following schematic? the real PN is LM5050-2.
Customer finds there is a 0.3% probability that Mos Q12/Q13 is damaged when carrying out hot plug in/out in parallel running. lm5050…
Part Number: UCC28083 Tool/software: Hi Team,
There is an issue that UCC28083 is not started up on the customer board. Their board specifications are as follows. And VDD pin voltage is measured to 12.5V, and current is measured to 0mA. Please check…
Part Number: UCC2808A-2 Tool/software: Hi,
Could you provide any manual or documents to design the circuit with UCC2808A-2? The details and examples more than datasheet are expected to fix the external constants.
Any equations to fix the external…
If that is the case, then submit a design review here when you are ready: https://www.ti.com/tool/SIMPLELINK-2-4GHZ-DESIGN-REVIEWS
I will review it with special attention to the RF path and give you feedback on how to avoid a Class II Permissive Change…
I've observed RTOS applications operating a 1 uA, the inclusion of RTOS should not be involved in higher current consumption numbers. Typically this could be caused by GPIO leakage. Have you submitted your design to SIMPLELINK-2-4GHZ-DESIGN-REVIEWS? …
Besides the ROM serial bootloader option, I recommend you submit your design to SIMPLELINK-2-4GHZ-DESIGN-REVIEWS so that the custom hardware may be reviewed and further JTAG locks are avoided.
You can also search for other E2E resolutions and determine…
Part Number: TPS51285A Other Parts Discussed in Thread: CSD87330Q3D Tool/software: Hello Sir/Mam
We are using TPS51285ARUKT along with MOSFET CSD87330Q3D.
1.5V current 7.9A
2.3.3V current 6.5A.
Could you please review and provide valuable…