Part Number: SK-AM62A-LP Tool/software: Hello!
We use the default SD card image burned on the SK-AM62A-LP E3 development board,
Start the development board and run it. In the cd/usr/lib directory, you can see the libraries containing OpenCV4.9 as follows…
Part Number: SK-AM62A-LP Other Parts Discussed in Thread: SYSCONFIG , UNIFLASH Tool/software: Hey all,
If someone could idiot-proof this for me I'd be grateful.
1. Can I output pwm on the 4 mcu+ timers?
2. I read that there can be resource reallocation…
Part Number: SK-AM62A-LP Tool/software: Hi,
I tested with AM62A PSDK 10.01.00.05, and the sigmoid issue occurred again.
SD card image : 10.01.00.05
edgeai-tidl-tools : 10_01_00_02
The issue occurs in one of the multiple sigmoid layers. Here are…
Part Number: SK-AM62A-LP Tool/software: Hello!
According to the document,
2. Getting started — Processor SDK AM62Ax Documentation
,we purchased IMX219 camera, and we verified the pin sequence;
After software startup, it can be recognized
…
Part Number: SK-AM62A-LP Tool/software: Hello Team, I am using gstreamer pipeline to stream h264 data. for that, I am using v4l2h264enc plugin. Command: gst-launch-1.0 -v v4l2src device=/dev/video-rpi-cam0 io-mode=dmabuf-import ! video/x-bayer, width=1920…
Part Number: SK-AM62A-LP Tool/software: Help with Real-Time Model Deployment and Network Streaming on AM62A LP
Hi, I am working with the AM62A LP board and would like to load my custom machine learning model onto the board. My goal is to achieve real…
Part Number: SK-AM62A-LP Tool/software: Hello,
we want to use use gstreamer pipeline from within docker on target. Gst plugins like tiovx should be useable.
Are there any ready docker images for target availbale?
If not, how to create docker image for…
Part Number: SK-AM62A-LP Other Parts Discussed in Thread: AM62P Tool/software: I need to connect 6 SPST Normally Open switches to the SK-AM62A-LP directly to the AM62 processor.
Which pins are free to use?
For some reason, the pins on the TM4C1294NCPDTT3R…