Part Number: SN65HVD1050 Hi team,
Could you kindly advise the Icc in the below conditions?
<Customer’s conditions>
- Node 30
- Termination 120 ohm (both end of the bus)
<Questions>
- Is the Icc of receiver node same with the Icc of recessive…
Part Number: SN65HVD1050-Q1 Hi Experts,
Good day. Client would like to use an alternative part.
To replace an existing CAN driver in a product, SN65HVD1050QDRQ1 is a good candidate, however the current part has pin 5 connected to Vcc. The datasheet…
Part Number: SN65HVD1050 Hi,
My customer has a question regarding the max and min signaling rate limitation of CAN bus transceiver.
For example, the recommended signaling rate for SN65HVD1050 is 20kbps to 1Mbps. Actually my customer is curious why…
Part Number: SN65HVD1050 Other Parts Discussed in Thread: TCAN1051-Q1
my customer is using SN65HVD1050DR for the BLDC Driving Board and found when the board just power on, the IC temp will rise to 50c degree very soon which even hotter than the…
Part Number: SN65HVD1050 Other Parts Discussed in Thread: TCAN1051-Q1 , TCAN1051V-Q1 , TCAN1042-Q1 What would happen if the Vref pin (pin 5) of SN65HVD1050 were to be back-driven by 3.3V? Since the functional block diagram doesn’t really indicate what…
Part Number: SN65HVD1050 Other Parts Discussed in Thread: TCAN1042V-Q1 Dear,
our client use TJA1049T, and we find SN65HVD1050 maybe can replace, but we saw the SN65HVD1050 cannot support standby mode and data rates up 1M.
have other suggestion, Please…
Hi Mihir,
SN65HVD1050 was tested according to the ISO7637-2 standard. This is an international testing standard that specifies the test setup and parameters in order to classify a device's protection rating. The information on pulse duration, timings…
Part Number: SN65HVD1050-EP Other Parts Discussed in Thread: SN65HVDA1050A-Q1 , SN65HVD1050-Q1 Hi Team,
Related to the question in the other thread:
In the datasheet, it is stated that it withstands voltage transients from –200 V to 200 V, according…
M. Arunkumar,
The choke we typically recommend is the ACT45B-101-2P. This has 100uH common-mode inductance, 5800 ohms impedance at 10MHz, a DC resistance of 2 ohms, rated voltage, and a rated current of 150mA. Another device we have used in our labs…
Part Number: SN65HVD1050 We have used SN65HVD1050MDREP for can bus communication in our designs ( electronic control unit, interface boards). Some of this component which have different voltage level do not work properly. For dominant bus states voltage…