Part Number: SN65HVD24 Hi
Used SN65HVD24, failing transmission of 300 meter cable at 4MHz rates.
At this point, a surge absorption part is used for requirement of IEC61000-4-5.
If absorption part is removed, transmission can be passed above…
Other Parts Discussed in Thread: SN65HVD24 Hi,
As below,for SN65HVD24 application,the current flow through Q2 and Q3,What's the maximum current that Q2 and Q3 will not be damaged?
Thanks!
Other Parts Discussed in Thread: SN65HVD24 Hi,
when I use SN65HVD24 to act as a receiver,it has a pulse on R pin about 0.8us before the valid data. The next scope is 2400bps.when I use 9600bps, all valid data become zero level.Is the circuIt's schematics…
Other Parts Discussed in Thread: SN65HVD24 , TXB0101 I submitted a techsupt request and was told instead to post here. That'd better mean that TI reps actually answer *here* if they don't answer directly...
I have a product under development that needs…
Part Number: SN65HVD23 Other Parts Discussed in Thread: SN65HVD24 , THVD1520 , THVD1550 , THVD1420 I'm trying to find an RS485 half-duplex transceiver that can handle over 100 nodes at a distance of over 100 meters and a speed over 10 Mbps (20-30 Mbps…
Awesome post, Figure 3 though doesn't really match the figure provided in SN65HVD24 datasheet. E.g. on Figure 3, for distance of 1000m, signaling rate is around 2Mbps. While in the datasheet, it shows below 1Mbps for 1000m. Thoughts?
Also, if Figure…
Hi Randy,
The pre-emphasis function is generally used to help extend the range of a link. Can you please let us know the data rate and cable length/type for your application? We can then check if THVD1552 may be suitable. Also, although we do not have…
Hi Max
Thank you for your reply.
I had forgotten that full-duplex transceiver is required.
SN65HVD24 can offer good performance, but it is half duplex device and it seems high class.
Let me close this thread relevant to TIDA.
Thank you for…
Part Number: SN65HVD82 Customer asks for sample code for SN65HVD82.
I found http://www.ti.com/tool/TIDA-00214?keyMatch=TIDA-00214&tisearch=Search-EN-Everything (RS-485 Bostterpack), based on SN65HVD24 .
Is this applicable for HVD82 or do we have something…
Hi Raghu,
I think your analysis is a very good starting point. (I say "starting point" here because it is difficult to arrive at an answer to this sort of issue without some kind of testing as well.) I think you may be overestimating the loss, though…