Part Number: SN65MLVD047 Tool/software: Hi Sir,
My customer need to extend its I2S length to 800mm for linking their two PCB boards. Are SN65MLVD047/48 good for 1.8V I2S application? Or any other suggestion for I2S buffer? Thanks for your kindly help…
Hello Srikanth,
Thanks for the clarification. The arrangement you described should work fine.
When connecting to the other board, you need to be careful with the termination scheme to make sure there is a 100 Ohm termination at the output of the SN65MLVD047…
Other Parts Discussed in Thread: SN65MLVD047 What's the difference between these two parts? Everything looks identical. Only slight differences I could find were small variations in the finish (gold/copper) ppm's in the environmental information, but…
Part Number: SN65LVDS31 Other Parts Discussed in Thread: SN65MLVD047 To Whom it May Concern,
I am currently reading Lit Number: SLLD009 (LVDS Application and Data Handbook) and was looking at the Precompensation in the Adjusting LVDS output levels section…
Part Number: SN65LVDT14 Other Parts Discussed in Thread: SN65MLVD047 , DS90LV011A Hello,
I was wondering for the SN65LVDT14 IC, whether there is a maximum rise and fall time on A and B inputs during transition? Or are the A and B differential inputs…
Hello,
60 ohms is very low and and will degrade the noise margins significantly (for any LVDS driver). As you said, it will put the system on the edge, especially if you add to that the fact that with multiple receivers and only one termination at…
Part Number: DS91M047 Other Parts Discussed in Thread: SN65MLVD047 , I am currently comparing the DS91M047 to the SN65MLVD047. The SN65MLVD047 shows a 30 to 55 ohm load (min/max) for Rl. The datasheet for the DS91M047 only shows characteristics at 50…
Other Parts Discussed in Thread: SN65MLVD2 , SN65MLVD047 , SN65LVDS4 Hi All,
In the current design I am using TX device: sn65mlvd047 , RX device: sn65mlvd2
I want to replace the RX device to sn65lvds4 from sn65mlvd2. Do you see any issues with this…
Thank you for these IBIS models.
One thing I don't understand. The two models say they are for the "D" SOIC package and the "DW" SOIC package. If you look at the datasheets for the SN65MLVD047 or 047A, they show a "D" SOIC-16 package and a "PW" TSSOP…