Part Number: SN74LV123A Tool/software: Dear Sir/ Madam,
We kindly ask you to update the MDS 875247653/3 and 153717170/8 due to the reason stated below.
Our ID is 14025!
Reason: The question for recyclate has not yet been answered
I`m sorry, but…
Part Number: SN74LV123A Tool/software: I see in the datasheet that the maximum value for the Cext capacitor is "No restriction". I tried simulating this in Altium Designer, and for larger capacitances, the voltage on the Rext/Cext pin did not reset to…
Part Number: SN74LV123A
Tool/software:
Hi support team all.
It seems that an order code SN74LV123APWE4 exists.
What does the "E4" in this code stand for?
A customer who placed an order with this order code in the past contacted us saying that…
Part Number: SN74LV123A-Q1 Tool/software: Hi experts!
I found two great reply about tw variation vs temperature. Tw is marked 0.9~1.1ms from the table and we can see the curve from firgure 15.
My question is does this test curve result considered…
Part Number: SN74LV123A-Q1 Other Parts Discussed in Thread: SN74LVC1G123 Tool/software: Hi Team,
I have searched related answers but it seems not accurate enough to solve these questions. Please help with these questions below:
[Q1]The three-temperature…
Part Number: SN74LV123A Tool/software: Hi,
I have any questions.
I have a question about the minimum input retriggering time.
Looking at the input and output relationship in Figure 7, I understand that if t_rr of /A is shorter than t_w, output…
Part Number: SN74LV123A Tool/software: Hi experts,
SN74LV123A Datasheet 7.3 recommended Operating Conditions shows Δ t/ Δ V Power-up ramp rate(min) = 1 [ms/V]
Q1. Just to confirm, it means we should take moer than 2ms when power up the SN74LV123A…
Part Number: SN74LV123A Tool/software: Hi experts,
The output pulse width t_w is determined by the following equation:
t_w = K × R_T × C_T
Is there an upper and lower limit for pulse width t_w that can be set? (For example, is it OK to set t_w=60s…
Part Number: SN74LV123A Other Parts Discussed in Thread: SN74LVC1G123 , Tool/software: Hi experts,
I want to know how to handle unused pins.
[Issues]
Connect Rext and Cext pins to GND -> abnormal heat generation
* Open Rext and Cext pins…
Part Number: SN74LV123A Hi all,
Our team has come across an issue which we've traced down to an unwanted activation of an output pulse from the SN74LV123A. The issue presents itself when the module in question is subjected to a quick power cycle. If…