Part Number: SN74LV123A Other Parts Discussed in Thread: SN74LVC1G123 Hello
I see that the SN74LV123ARGYR is Obsolete and I am looking for a replacement. I see that it is in a VQFN package, and that none of the active OPNs for that device come in that…
Part Number: SN74LV123A I am trying to do a last time buy for my design. My part number is 74LV123ARGYR and was wondering what the differences are (if any) between 74LV123AR GYR and 74LV123AR GYRG4. Looking at data sheet, I cannot tell what the G4 suffix…
Part Number: SN74LV123A Hi team,
In the datasheet, K-Vcc is spec'd only for CT=1000pF, 0.01uF, 0.1uF and 1uF. But my customer wants to use CT=10uF with Vcc=3.3V or 5V. Could you show us the characteristic for CT=10uF?
Regards,
Ohashi
Part Number: SN74LV123A-Q1 Hi ,
The customer used SN74LV123ATPWRG4Q1 before, do you recommend a new product to replace it?
What is the difference between SN74LV123ATPWRQ1 and SN74LV123ATPWRG4Q1? Are compatible replacements available?
Thanks~
Part Number: SN74LV123A-Q1 Hello,
While referencing the datasheet for the SN74LV123A-Q1 monostable multivibrator, we noticed some discrepancies and we need some clarification. The pin function table (page 3) shows 1B should be LOW when trigger input…
Part Number: SN74LV123A Hello,
We are using SN74LV123A IC in our design. we are expecting the outputs as truth table highlighted per attached image.
Our circuit is as below attached image.
Input B is as shown in the attached image below. with…
Part Number: SN74LV123A Hi,
We use the Buffer IC SN74LVC8T245RHLR in our design.
I am wrongly connected the Input voltage Range is 3.3V , but the VCC is given as 1.8V.
Shall we proceed with input voltage is more than the VCC?
Kindly confirm…
Part Number: SN74LV123A In sn74lv123A datasheet their capacitor graph is not mentioned properly.so there is a little confusion while designing it can you please help me to design.
And thee is not proper formula for SN74lv123a to select Rext and Cext…
Part Number: SN74LV123A
Hi,
I am working on a retriggerable multivibrator circuit, with a pulse with of 20ms for the rising edge of the pulse. I used the value of k=0.9, as the input voltage value is 3.3V. Did not work, when tried simulating in…