Part Number: SN74LVC1G11 Hello,
The SN74LVC1G11 states 10uA max for quiesent current.
Would you be able to share any real-world measurements? We're most interested in 3.3Vin.
Thank you, Keith
Part Number: SN74LVC1G11-Q1 Other Parts Discussed in Thread: SN74LVC1G11
Tool/software:
Hi
looking at TI SN74LVC1G11-Q1, its appears as -40 to 85 deg but i think its a mistake as SN74LVC1G11 that is not automotive have temperature range of -40…
Part Number: SN74LVC1G11 Need automotive grade supporting alternate parts for the following list.
SN74AHC1G02DRLR SN74LVC1G08DBVRE4 SN74CB3Q3257PWR SN74AVC4T245RSVR SN74LVC1G17DCKR SN74LVC1G11DCKR
Foot prints and pin compatibility are preferred.
Part Number: SN74LVC1G11 Tool/software: Hi
We are using SN74LVC1G11DBVR in our design. We have supply at 5V for this IC. We have connected power good signals to this IC. each of the input power good has pull up to 5V(available in a different sheet)…
Part Number: SN74LVC1G11 Tool/software: It doesn't seem to allow 3.3V input.
The SN74LVC1G11 doesn't seem to have a positive clamp diode.
What is acceptable?
Part Number: SN74LVC1G11 Tool/software: Hi Everyone,
Using SN74LVC1G11 to feed an RC network - R = 22Ohm, C = 470pF - this will result in peak current of VCC/22 = 5/22 = 227mA for a very short time.
Will this high peak current allowable? will we need…
Part Number: SN74LVC1G11 Tool/software: Hi
I noticed that the footprint and the STEP file in the web site is incorrect the sot23-6 pads, width and length.
for exempla the pads in the data sheet is 0.9*0.4 and not as in the downloaded design that is…
Part Number: SN74LVC1G11 Tool/software: HI Team,
For this 2 input AND gate there is no data given for VOH and VOL for VDD=3.3V and VDD=5V??
Similarly for SN74LVC1GU04DBVR (NOT gate), SN74LVC1G11DCKR ( 3 input AND gate ) and SN74LVC1G34DSFR ( 1bit…
Part Number: SN74LVC1G11-Q1 Hi Expert,
My customer is using SN74LVC1G11-q1 in their project.
Would you mind helping me to identify the TJ of SN74LVC1G11-Q1?
I only find the value of TA in their project.
Kind Regards
Imelda
Part Number: SN74LVC1G11 Tool/software: Hi Team,
I am interfacing AND gate (SN74LVC1G11DCKR) Output to a NOT gate(SN74LVC1GU04DBVR) input.
component 1
VOH1 (min) (V)
VOL1 (MAX) (V)
VIH1 (MIN) (V)
VIL1 (MAX) (V)
Component 2
VOH2 …