Part Number: SN74LVC1G14 Dears:
Pls. refer the below schematic, and customer wants to replace IC3 TC4S584F.
However, our PN will be burned.
Pls. kindly help to check the below schematic, and give some advice or other PN to replace TC4S584F.
Part Number: SN74LVC1G14-Q1 Hello,
I noticed that there are several part markings for this device available.
(C145, C14F, C14J, C14K, C14R) (C14H, C14S)..
Can you give some details on the meaning of this marking? What is the difference between…
Part Number: SN74LVC1G14-EP Hello,
We are considering SN74LVC1G14-EP component as our Schitt-Trigger Inverter.
Here is the example we would like to show the example reagarding over-voltage tolerance inputs.
eg: Supply Voltage Vcc = 3.3V
Input…
Part Number: SN74LVC1G14-Q1 Other Parts Discussed in Thread: SN74AUC245 , SN74AUC244 Hi Experts,
I'm looking for some single bit buffer that could support tpd less than 1ns. Not sure if any standard logic component could support this. or any thing else…
Part Number: SN74LVC1G14 Hi dear supporting team,
customer is requesting for the recommended Tj which is allowed for long term operating for SN74LVC1G14, d/s only have absolute rating. could you help provide it? and BTW, is there FIT data related with…
Part Number: SN74LVC1G14 Hi Expert,
In datasheet, the operating temperature is specified as 85 degree.
However, in the website of sample, the temperature is -40 to 125. Why the same device has different operating temperature? In what case, the…
Part Number: SN74LVC1G14-Q1 Other Parts Discussed in Thread: TLV3201-Q1 , SN74AUP1T34-Q1 , TLV3201 , TLV3501 , TLV3501A-Q1 , SN74LVC1G04-Q1 Hi team,
I would like to translate 0.8Vpp TCXO output clock to 1.8V CMOS level input for TDA2x.
TCXO output…
Part Number: SN74LVC1G14 Other Parts Discussed in Thread: SN74LVC1G126 , What happens to the output of this device during power up/down? I am using this device to control a critical signal and if the output signal is low at the wrong time it will cause…
Hi Pradeep,
The device may work above 6.5 Volts with current limiting resistors however once the device goes above the Absolute Max voltage you void the warranty on the device and we cannot guarantee any of our specs on the data sheet.
Can you go…