Part Number: SN74LVC1G240 Dear Team,
I am controlling two MUX's using SN74LVC1G240. During power on all the MUX's are disabled.
When 8:1 MUX is enabled the 4:1 MUX should be disabled.
For implementing this logic I used SN74LVC1G240 for controlling…
Part Number: SN74LVC1G240 We are interested to understand which max current consumption to expect from this component. The datasheet lists all figures, but we wanted to post a question to ensure that we do not misunderstand.
During normal use the device…
Part Number: SN74LVC1G240 Hi,
We have a specific scenario that we would like to ask about with regards to the expected SN74LVC1G240 behavior.
The output (Y) is connected to the gate of an nFET with 1 mega ohm pull-down and 10 uF (actual) capacitance…
Part Number: SN74LVC1G240 Please provide documentation for the package thermal impedance for the SN74LVC1G240 in the DRY and DSF packages.
Page 2 of the datasheet shows the package thermal impedance for the DBV, DCK, and YZP packages. The datasheet…
Part Number: SN74LVC1G240 Other Parts Discussed in Thread: SN74LVC1G02 , SN74AHC02 , UCC23511 , SN74LV541A , SN74LV540A In the Truth table, when the /OE pin is high, the output is high-impedance. How to make that when /OE pin is high, the output is LOW…
Part Number: SN74LVC1G240 Other Parts Discussed in Thread: SN74LXC2T45 , SN74LV1T125 , SN74LV1T04 Hi ,
control signal pin1 & pin2 is 3.3V, when Vcc =5V, pin1 is pulled 3.3V (off ) ,the current is high, about 5mA; did some test, i found that it is normal…
Part Number: SN74LVC1G240 The data sheets indicate a minimum value of resistance to connect OE to VCC. But there is no
information on how to calculate this. So where is the formula?
Both the low and high level output current have multiple values for…
Part Number: SN74LVC1G240 Other Parts Discussed in Thread: SN74LVC1G02 Hi Team,
In datasheet listed that when /OE pin is high and Output would be high impendence. Due to the system needs to make sure the output is low during system bring up and keep…
Part Number: SN74LVC1G240 Hi Team,
My Customer is asking if the DCK package of SN74LVC1G240 pin configuration as stated in our datasheet is correct? They built 100 PCBs using the DCK package and none of them work. They desolder and put the larger DBV…