Part Number: TCAN1042HGV-Q1 Hi, TI support Team
A request for schematic review has been received from a customer.
I request a review of the circuit diagram below.
Thanks.
Regards,
MJ
Part Number: TCAN1042HGV-Q1 Hello team,
I want to check with you, if we can also connect the STB directly to GND if not needed or do we need a 10k Ohm resistor? Thanks,
Matt
Part Number: TCAN1042HGV-Q1 Hi TI teams
In the datasheet of TCAN1042HGV-Q1, there is an option for ESD.
Do you have the recommended component for ESD?
or any specification recommended?
Thanks
Lukas
Part Number: TCAN1042HGV Hi team,
My customer met Pin3 Burned issue in low temperature tests.
1. Failure happened during PP, failure rate 10/20, all chips' PIN3 are burned.
2. In room temp, communication is normal, but when the temp decreased to…
Part Number: TCAN1042HGV-Q1 Other Parts Discussed in Thread: TCAN1051 To whom it may concern,
Due to supply chain issues I am trying to find an alternate to the TCAN1042HGVDRBRQ1 part. I see that the TCAN1051 is available to purchase with same footprint…
Part Number: TCAN1042HGV-Q1 Hi TI team,
We are currently working on a project that has a really tight sleep current requirement and we request your help in finding out leakage current from TCAN IC. During the sleep mode of our device, only the 3.3V…
Part Number: TCAN1042HGV-Q1 Other Parts Discussed in Thread: LM5160 , TCAN1043 , ISO7742
Hi Team,
The customer is using the TCAN1042HGV-Q1 for the electric compressor inverter.
Even if the secondary circuit enters Sleep mode and does not consume…
Part Number: TCAN1042HGV
Hi Interface Experts,
My customer is designing a TCAN1042 with split termination using 60 ohms and a CSPLIT cap as shown in the datasheet figure 17.
After reading this post https://e2e.ti.com/support/interface/f/138…