Part Number: TUSB8041 Other Parts Discussed in Thread: TIDA-00288 Ti 工程师您好,
我 参考TIDA-00288 制作了一款TUSB8041hub 电脑端无法识别2.0端口。3.0端口可以正常使用
如下是电路原理图
更换过其他电脑测试,电脑端显示
请问是否有电脑端驱动程序或者配置工具才能显示USB2.0设备?
Part Number: TUSB8041 Other Parts Discussed in Thread: TIDA-00288 Hi team,
I am working with one of my customer & they want to use TUSB8041 - USB3.0 Hub.
Their query is related to throughput.
Practically what throughput can be expected from TUSB8041…
Hi,
To customize the registers inside of TUSB8042, customer must use I2C or SMBus. Option 2 is correct. I believe TIDA-00288 uses default register settings of TUSB8041, a custom USB Hub driver is not required.
What is your customer trying to achieve…
Hi Eric ,
Once again Thank you for the quick response !!
Ok , but Gerber which is shared requires changes in Minimum Spacing and trace size as requested from our PCB fabricator.
but I see for TIDA-00288 TI-design has shared the .brd files in…
Other Parts Discussed in Thread: TIDA-00288 , TUSB8041EVM My first idea was to put 0402 10nF decoupling caps on the same side as the IC, close to the power pins, but on the TUSB8041EVM and TIDA-00288 I see all the caps on the opposite side.
Is there…
Part Number: TUSB8041 Other Parts Discussed in Thread: TIDA-00288 , Hello,
I am implementing an on board USB3 hub on a board that we are designing using a TUSB8401 device and basing it on the TIDA-00288 4-Port USB 3.0 Hub Reference Design.
I have…
Other Parts Discussed in Thread: TUSB8041-Q1 , TIDA-00288 , TUSB8041 I designed a USB HUB board with TUSB8041-Q1, 3 down-stream USB 3.0 ports and 1 down-stream USB 2.0 port. I connected two high resolution USB 3.0 cameras from the following link, with…
Hello Chethan,
I apologize for the late reply. For some reason your post did not originally come up on our feed of new questions.
1. I cannot comment on the compatibility of our part with the USB2514B. To make sure the USB charger and the controller…
Other Parts Discussed in Thread: TUSB8041-Q1 Hi
I am in an early stage of designing a USB 3.0 hub. I was thinking of using tusb8041-q1 automotive grade for design as my product have a fair share of automotive market. I have couple of qustions
1. What…